#include <mcuxClToolchain.h>
#include <mcuxClCore_Examples.h>
#include <mcuxClExample_Session_Helper.h>
#include <mcuxClExample_RNG_Helper.h>
#define MCUXCLMAC_CPU_WA_BUFFER_SIZE (MCUXCLMAC_MAX_CPU_WA_BUFFER_SIZE + MCUXCLRANDOM_NCINIT_WACPU_SIZE)
static const uint8_t data[40] = {
0x6b, 0xc1, 0xbe, 0xe2, 0x2e, 0x40, 0x9f, 0x96,
0xe9, 0x3d, 0x7e, 0x11, 0x73, 0x93, 0x17, 0x2a,
0xae, 0x2d, 0x8a, 0x57, 0x1e, 0x03, 0xac, 0x9c,
0x9e, 0xb7, 0x6f, 0xac, 0x45, 0xaf, 0x8e, 0x51,
0x30, 0xc8, 0x1c, 0x46, 0xa3, 0x5c, 0xe4, 0x11
};
static const uint8_t keyDataAes128[16] = {
0x2b, 0x7e, 0x15, 0x16, 0x28, 0xae, 0xd2, 0xa6,
0xab, 0xf7, 0x15, 0x88, 0x09, 0xcf, 0x4f, 0x3c
};
static const uint8_t cmacReferenceAes128[16] = {
0xdf, 0xa6, 0x67, 0x47, 0xde, 0x9a, 0xe6, 0x30,
0x30, 0xca, 0x32, 0x61, 0x14, 0x97, 0xc8, 0x27
};
MCUXCLEXAMPLE_FUNCTION(mcuxClMacModes_Cmac_Aes128_Multipart_example)
{
mcuxClSession_Descriptor_t sessionDesc;
MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_SESSION(session, MCUXCLMAC_CPU_WA_BUFFER_SIZE, 0u);
uint32_t keyDesc[MCUXCLKEY_DESCRIPTOR_SIZE_IN_WORDS];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
session,
key,
keyDataAes128,
sizeof(keyDataAes128))
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUXCLEXAMPLE_INITIALIZE_PRNG(session);
ALIGNED uint8_t ctxBuf[MCUXCLMAC_CONTEXT_SIZE];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
uint8_t macData[sizeof(cmacReferenceAes128)];
session,
ctx,
key,
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
session,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by mcuxClMac_init")
ctx,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
dataBuff,
5u)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
session,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by mcuxClMac_init")
ctx,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
dataBuff,
sizeof(data) - 5u)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
uint32_t macSize = 0u;
session,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by mcuxClMac_init")
ctx,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
macDataBuf,
&macSize)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(!mcuxClExample_Session_Clean(session))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if (macSize != sizeof(cmacReferenceAes128))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if (!mcuxClCore_assertEqual(macData, cmacReferenceAes128, sizeof(cmacReferenceAes128)))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
return MCUXCLEXAMPLE_STATUS_OK;
}
Top-level include file for the mcuxClAes component.
Top-level include file for the mcuxClBuffer component.
Definition of function identifiers for the flow protection mechanism.
Top-level include file for the mcuxClKey component.
Top-level include file for the mcuxClMac component.
Top-level include file for the mcuxClMacModes component.
Top-level include file for the mcuxClSession component.
Provides the API for the CSSL flow protection mechanism.
static const mcuxClKey_Type_t mcuxClKey_Type_Aes128
Key type pointer for AES-128 based keys.
Definition mcuxClAes_KeyTypes.h:51
#define MCUXCLBUFFER_INIT(name, info, ptr, size)
Initialize an input/output buffer (mcuxCl_Buffer_t).
Definition mcuxClBuffer.h:67
#define MCUXCLBUFFER_INIT_RO(name, info, ptr, size)
Initialize an input buffer (mcuxCl_InputBuffer_t) with plain CPU handling.
Definition mcuxClBuffer.h:84
#define MCUXCLBUFFER_UPDATE(name, offset)
Update the buffer pointer with the given offset.
Definition mcuxClBuffer.h:201
#define MCUXCLKEY_STATUS_OK
Key operation successful.
Definition mcuxClKey_Constants.h:40
mcuxClKey_Status_t mcuxClKey_init(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClKey_Type_t type, const uint8_t *pKeyData, uint32_t keyDataLength)
Initializes a key handle.
mcuxClKey_Descriptor_t *const mcuxClKey_Handle_t
Key handle type.
Definition mcuxClKey_Types.h:91
#define MCUXCLMAC_STATUS_OK
Blocking operation finished successfully.
Definition mcuxClMac_Constants.h:36
mcuxClMac_Status_t mcuxClMac_process(mcuxClSession_Handle_t session, mcuxClMac_Context_t *const pContext, mcuxCl_InputBuffer_t pIn, uint32_t inLength)
Data processing for a multipart MAC computation.
mcuxClMac_Status_t mcuxClMac_init(mcuxClSession_Handle_t session, mcuxClMac_Context_t *const pContext, mcuxClKey_Handle_t key, mcuxClMac_Mode_t mode)
Initialization for a multipart MAC computation.
mcuxClMac_Status_t mcuxClMac_finish(mcuxClSession_Handle_t session, mcuxClMac_Context_t *const pContext, mcuxCl_Buffer_t pMac, uint32_t *const pMacLength)
Finalize a MAC generation for a multipart MAC computation.
struct mcuxClMac_Context mcuxClMac_Context_t
Mac context type.
Definition mcuxClMac_Types.h:98
static mcuxClMac_Mode_t mcuxClMac_Mode_CMAC
AES-CMAC mode.
Definition mcuxClMacModes_Modes.h:48
mcuxClSession_Descriptor_t *const mcuxClSession_Handle_t
Type for mcuxClSession Handle.
Definition mcuxClSession_Types.h:98
#define MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(...)
Call a flow protected function and check the protection token.
Definition mcuxCsslFlowProtection.h:623
#define MCUX_CSSL_FP_FUNCTION_CALLED(...)
Expectation of a called function.
Definition mcuxCsslFlowProtection.h:777
#define MCUX_CSSL_FP_FUNCTION_CALL_END(...)
End a function call section started by MCUX_CSSL_FP_FUNCTION_CALL_BEGIN.
Definition mcuxCsslFlowProtection.h:658