MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClHmac_Sw_Multipart_example.c

mcuxClHashModes example application

mcuxClHashModes example application

/*--------------------------------------------------------------------------*/
/* Copyright 2023-2025 NXP */
/* */
/* NXP Confidential and Proprietary. This software is owned or controlled */
/* by NXP and may only be used strictly in accordance with the applicable */
/* license terms. By expressly accepting such terms or by downloading, */
/* installing, activating and/or otherwise using the software, you are */
/* agreeing that you have read, and that you agree to comply with and are */
/* bound by, such license terms. If you do not agree to be bound by the */
/* applicable license terms, then you may not retain, install, activate or */
/* otherwise use the software. */
/*--------------------------------------------------------------------------*/
#include <mcuxClToolchain.h>
#include <mcuxClCore_Examples.h> // Defines and assertions for examples
#include <mcuxClExample_Session_Helper.h>
#include <mcuxClKey.h>
#include <mcuxClSession.h>
#include <mcuxClCore_FunctionIdentifiers.h> // Code flow protection
#include <mcuxClMac.h> // Interface to the entire mcuxClMac component
#include <mcuxClHmac.h> // Interface to the entire mcuxClHmac component
#include <mcuxClHash.h>
#include <mcuxClExample_RNG_Helper.h>
/* Example (unpadded) key. */
static const ALIGNED uint8_t hmac_key[] = {
0x00u, 0x11u, 0x22u, 0x33u, 0x44u, 0x55u, 0x66u, 0x77u,
0x88u, 0x99u, 0xaau, 0xbbu, 0xccu, 0xddu, 0xeeu, 0xffu,
0x00u, 0x11u, 0x22u, 0x33u, 0x44u, 0x55u, 0x66u, 0x77u,
0x88u, 0x99u, 0xaau, 0xbbu, 0xccu, 0xddu, 0xeeu, 0xffu
};
/* Example inputs to the HMAC function. */
static const ALIGNED uint8_t hmac_input_part1[] = {
0x00u, 0x9fu, 0x5eu, 0x39u, 0x94u, 0x30u, 0x03u, 0x82u,
0x50u, 0x72u, 0x1bu, 0xe1u, 0x79u, 0x65u, 0x35u, 0xffu,
0x21u, 0xa6u, 0x09u, 0xfdu, 0xf9u, 0xf0u, 0xf6u, 0x12u,
0x66u, 0xe3u
};
static const ALIGNED uint8_t hmac_input_part2[] = {
0xafu, 0x75u, 0xd7u, 0x04u, 0x31u, 0x7du, 0x55u, 0x06u,
0xf8u, 0x06u, 0x5cu, 0x48u, 0x72u, 0x18u, 0xe9u, 0x9eu,
0xb4u, 0xc3u, 0xd4u, 0x54u, 0x6cu, 0x4du, 0x60u, 0x70u,
0x16u, 0x90u, 0x11u, 0x38u, 0x73u, 0x9du, 0xbdu, 0xf4u,
0x37u, 0xa5u, 0xe6u, 0xf5u, 0x02u, 0x1au
};
/* Example reference HMAC. */
static const ALIGNED uint8_t hmac_output_reference[MCUXCLHASH_OUTPUT_SIZE_SHA_256] = {
0x06u, 0xb8u, 0xb8u, 0xc3u, 0x21u, 0x79u, 0x15u, 0xbeu,
0x0bu, 0x0fu, 0x86u, 0x90u, 0x4fu, 0x76u, 0x74u, 0x1bu,
0x1bu, 0xe2u, 0x86u, 0x79u, 0x38u, 0xf4u, 0xf0u, 0x5du,
0x34u, 0x15u, 0xbbu, 0x36u, 0x8fu, 0x4au, 0x57u, 0xfbu
};
MCUXCLEXAMPLE_FUNCTION(mcuxClHmac_Sw_Multipart_example)
{
/**************************************************************************/
/* Preparation */
/**************************************************************************/
/* Allocate and initialize session / workarea */
mcuxClSession_Descriptor_t sessionDesc;
mcuxClSession_Handle_t session = &sessionDesc;
/* Allocate and initialize session / workarea */
MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_SESSION(session, MCUXCLEXAMPLE_MAX_WA(MCUXCLHMAC_MAX_CPU_WA_BUFFER_SIZE, MCUXCLRANDOM_NCINIT_WACPU_SIZE), 0u);
/* Initialize the PRNG */
MCUXCLEXAMPLE_INITIALIZE_PRNG(session);
/**************************************************************************/
/* Key setup */
/**************************************************************************/
/* Create and initialize mcuxClKey_Descriptor_t structure. */
uint32_t keyDesc[MCUXCLKEY_DESCRIPTOR_SIZE_IN_WORDS];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(keyInit_result, keyInit_token, mcuxClKey_init(
/* mcuxClSession_Handle_t pSession: */ session,
/* mcuxClKey_Handle_t key: */ key,
/* const mcuxClKey_Type* type: */ mcuxClKey_Type_Hmac_variableLength,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_DISCARD_CONST("Required by API function")
/* mcuxCl_Buffer_t pKeyData: */ (uint8_t *) hmac_key,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_DISCARD_CONST()
/* uint32_t keyDataLength: */ sizeof(hmac_key)));
if((MCUX_CSSL_FP_FUNCTION_CALLED(mcuxClKey_init) != keyInit_token) || (MCUXCLKEY_STATUS_OK != keyInit_result))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/**************************************************************************/
/* Generate an HMAC mode containing the hash algorithm */
/**************************************************************************/
ALIGNED uint8_t hmacModeDescBuffer[MCUXCLHMAC_HMAC_MODE_DESCRIPTOR_SIZE];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
mcuxClMac_CustomMode_t mode = (mcuxClMac_CustomMode_t) hmacModeDescBuffer;
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(hashCreateMode_result, hashCreateMode_token, mcuxClHmac_createHmacMode(
/* mcuxClMac_CustomMode_t mode: */ mode,
/* mcuxClHash_Algo_t hashAlgorithm: */ mcuxClHash_Algorithm_Sha256)
);
if((MCUX_CSSL_FP_FUNCTION_CALLED(mcuxClHmac_createHmacMode) != hashCreateMode_token) || (MCUXCLMAC_STATUS_OK != hashCreateMode_result))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/**************************************************************************/
/* HMAC computation */
/**************************************************************************/
/* Output buffer for the computed MAC. */
uint8_t result[MCUXCLHMAC_MAX_OUTPUT_SIZE];
MCUXCLBUFFER_INIT_RW(resultBuf, session, result, sizeof(result));
uint32_t result_size = 0u;
MCUXCLBUFFER_INIT_RO(inputBuf1, session, hmac_input_part1, sizeof(hmac_input_part1));
MCUXCLBUFFER_INIT_RO(inputBuf2, session, hmac_input_part2, sizeof(hmac_input_part2));
ALIGNED uint8_t ctxBuf[MCUXCLHMAC_CONTEXT_SIZE_SW];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
/* mcuxClSession_Handle_t session: */ session,
/* mcuxClMac_Context_t * const pContext: */ ctx,
/* const mcuxClKey_Handle_t key: */ key,
/* mcuxClMac_Mode_t mode: */ mode)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/* mcuxClSession_Handle_t session: */ session,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by mcuxClMac_init")
/* mcuxClMac_Context_t * const pContext: */ ctx,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
/* mcuxCl_InputBuffer_t pIn: */ inputBuf1,
/* uint32_t inLength: */ sizeof(hmac_input_part1))
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/* mcuxClSession_Handle_t session: */ session,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by mcuxClMac_init")
/* mcuxClMac_Context_t * const pContext: */ ctx,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
/* mcuxCl_InputBuffer_t pIn: */ inputBuf2,
/* uint32_t inLength: */ sizeof(hmac_input_part2))
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/* mcuxClSession_Handle_t session: */ session,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by mcuxClMac_init")
/* mcuxClMac_Context_t * const pContext: */ ctx,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
/* mcuxCl_Buffer_t pMac: */ resultBuf,
/* uint32_t * const pMacLength: */ &result_size)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/**************************************************************************/
/* Verification */
/**************************************************************************/
/* Compare the output size with the expected MAC size */
if(sizeof(hmac_output_reference) != result_size)
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/* Compare the result to the reference value. */
if(!mcuxClCore_assertEqual(hmac_output_reference, result, sizeof(hmac_output_reference)))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/**************************************************************************/
/* Cleanup */
/**************************************************************************/
/* Clean-up and destroy the session. */
if(!mcuxClExample_Session_Clean(session))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
return MCUXCLEXAMPLE_STATUS_OK;
}
Definition of function identifiers for the flow protection mechanism.
Top-level include file for the mcuxClHash component.
Top-level include file for the mcuxClHashModes component.
Top-level include file for the mcuxClHmac component.
Top-level include file for the mcuxClKey component.
Top-level include file for the mcuxClMac component.
Top-level include file for the mcuxClSession component.
Provides the API for the CSSL flow protection mechanism.
#define MCUXCLBUFFER_INIT_RW(name, info, ptr, size)
Initialize an input/output buffer (mcuxCl_Buffer_t) with plain CPU handling.
Definition mcuxClBuffer.h:101
#define MCUXCLBUFFER_INIT_RO(name, info, ptr, size)
Initialize an input buffer (mcuxCl_InputBuffer_t) with plain CPU handling.
Definition mcuxClBuffer.h:84
static mcuxClHash_Algo_t mcuxClHash_Algorithm_Sha256
Sha-256 algorithm descriptor Sha-256 hash calculation using the Hash functionality SGI.
Definition mcuxClHashModes_Algorithms.h:96
#define MCUXCLHASH_OUTPUT_SIZE_SHA_256
SHA-256 output size: 256 bit (32 bytes).
Definition mcuxClHashModes_Constants.h:38
mcuxClMac_Status_t mcuxClHmac_createHmacMode(mcuxClMac_CustomMode_t mode, mcuxClHash_Algo_t hashAlgorithm)
This function creates a HMAC mode descriptor for software implementations of HMAC.
static const mcuxClKey_Type_t mcuxClKey_Type_Hmac_variableLength
Key type pointer for HMAC keys with variable length.
Definition mcuxClHmac_KeyTypes.h:47
#define MCUXCLKEY_STATUS_OK
Key operation successful.
Definition mcuxClKey_Constants.h:40
mcuxClKey_Status_t mcuxClKey_init(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClKey_Type_t type, const uint8_t *pKeyData, uint32_t keyDataLength)
Initializes a key handle.
mcuxClKey_Descriptor_t *const mcuxClKey_Handle_t
Key handle type.
Definition mcuxClKey_Types.h:91
#define MCUXCLMAC_STATUS_OK
Blocking operation finished successfully.
Definition mcuxClMac_Constants.h:36
mcuxClMac_Status_t mcuxClMac_process(mcuxClSession_Handle_t session, mcuxClMac_Context_t *const pContext, mcuxCl_InputBuffer_t pIn, uint32_t inLength)
Data processing for a multipart MAC computation.
mcuxClMac_Status_t mcuxClMac_init(mcuxClSession_Handle_t session, mcuxClMac_Context_t *const pContext, mcuxClKey_Handle_t key, mcuxClMac_Mode_t mode)
Initialization for a multipart MAC computation.
mcuxClMac_Status_t mcuxClMac_finish(mcuxClSession_Handle_t session, mcuxClMac_Context_t *const pContext, mcuxCl_Buffer_t pMac, uint32_t *const pMacLength)
Finalize a MAC generation for a multipart MAC computation.
mcuxClMac_ModeDescriptor_t *const mcuxClMac_CustomMode_t
MAC custom mode/algorithm type.
Definition mcuxClMac_Types.h:75
struct mcuxClMac_Context mcuxClMac_Context_t
Mac context type.
Definition mcuxClMac_Types.h:98
mcuxClSession_Descriptor_t *const mcuxClSession_Handle_t
Type for mcuxClSession Handle.
Definition mcuxClSession_Types.h:98
#define MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(...)
Call a flow protected function and check the protection token.
Definition mcuxCsslFlowProtection.h:623
#define MCUX_CSSL_FP_FUNCTION_CALLED(...)
Expectation of a called function.
Definition mcuxCsslFlowProtection.h:777
#define MCUX_CSSL_FP_FUNCTION_CALL_END(...)
End a function call section started by MCUX_CSSL_FP_FUNCTION_CALL_BEGIN.
Definition mcuxCsslFlowProtection.h:658