MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClSession_cleanupOnError_example.c

Example for the mcuxClSession CleanupOnError function.

Example for the mcuxClSession CleanupOnError function.

/*--------------------------------------------------------------------------*/
/* Copyright 2025 NXP */
/* */
/* NXP Confidential and Proprietary. This software is owned or controlled */
/* by NXP and may only be used strictly in accordance with the applicable */
/* license terms. By expressly accepting such terms or by downloading, */
/* installing, activating and/or otherwise using the software, you are */
/* agreeing that you have read, and that you agree to comply with and are */
/* bound by, such license terms. If you do not agree to be bound by the */
/* applicable license terms, then you may not retain, install, activate or */
/* otherwise use the software. */
/*--------------------------------------------------------------------------*/
#include <mcuxClToolchain.h>
#include <mcuxClSession.h>
#include <mcuxClBuffer.h>
#include <mcuxClKey.h>
#include <mcuxClHash.h>
#include <mcuxClEcc.h>
#include <mcuxClCore_Examples.h>
#include <mcuxClExample_Session_Helper.h>
#include <mcuxClCore_FunctionIdentifiers.h> // Code flow protection
static const uint8_t data[] = {
0xCAu, 0x83u, 0x5Fu, 0x5Bu, 0x0Bu, 0x44u, 0x33u, 0x32u,
0x11u, 0x4Eu, 0xEAu, 0xA5u, 0x9Au, 0xE5u, 0x56u, 0x7Eu,
0x4Fu, 0x86u, 0xAFu, 0x72u, 0xF1u, 0x1Cu, 0xB4u, 0xE6u,
0x71u, 0xD9u, 0x13u, 0xDEu, 0x03u, 0xD4u, 0xC5u, 0xB7u
};
static const ALIGNED uint8_t pubKeyBytes[MCUXCLECC_WEIERECC_NIST_P256_SIZE_PUBLICKEY] = {
0xE8u, 0x19u, 0xC6u, 0x90u, 0x80u, 0xFEu, 0x45u, 0x2Fu,
0x12u, 0x3Du, 0xA0u, 0x2Cu, 0xC7u, 0xB1u, 0x8Du, 0x54u,
0xE1u, 0x83u, 0x95u, 0x82u, 0xF9u, 0xF4u, 0x0Du, 0x90u,
0xBBu, 0x77u, 0xF3u, 0x8Cu, 0x60u, 0x84u, 0x37u, 0xC6u,
0x85u, 0x62u, 0xAAu, 0xA4u, 0x8Du, 0x2Du, 0x61u, 0x1Fu,
0xF1u, 0xEFu, 0x58u, 0x50u, 0x6Bu, 0x08u, 0xC2u, 0x62u,
0x01u, 0x2Bu, 0xC0u, 0xC1u, 0x3Eu, 0xD7u, 0x37u, 0x72u,
0x44u, 0x65u, 0xB3u, 0x2Cu, 0x02u, 0x79u, 0x85u, 0x9Au
};
static const uint8_t signature[MCUXCLECC_WEIERECC_NIST_P256_SIZE_SIGNATURE] = {
//R
0x28u, 0xF7u, 0xA7u, 0x1Au, 0xADu, 0xEAu, 0x35u, 0x2Au,
0x41u, 0x33u, 0xB5u, 0x3Au, 0x79u, 0x1Cu, 0x69u, 0x33u,
0x38u, 0x2Au, 0xE3u, 0x74u, 0xBDu, 0xA7u, 0xB6u, 0x50u,
0x20u, 0xE0u, 0xF6u, 0x8Du, 0x1Bu, 0x1Bu, 0x35u, 0x46u,
//S
0xF8u, 0x61u, 0x71u, 0x93u, 0xA9u, 0x3Au, 0xB6u, 0x22u,
0xD0u, 0x03u, 0xBFu, 0xC0u, 0x77u, 0xB8u, 0x41u, 0xD9u,
0x91u, 0xDFu, 0xFCu, 0xC5u, 0xEFu, 0x34u, 0xE2u, 0x53u,
0xBFu, 0xB5u, 0x9Eu, 0xA7u, 0xC7u, 0xAFu, 0x40u, 0x13u
};
#define MAX_CPUWA_SIZE MCUXCLSIGNATURE_VERIFY_ECDSA_WACPU_SIZE
#define MAX_PKCWA_SIZE MCUXCLSIGNATURE_VERIFY_ECDSA_WAPKC_SIZE_256
MCUXCLEXAMPLE_FUNCTION(mcuxClSession_cleanupOnError_example)
{
/**************************************************************************/
/* Preparation */
/**************************************************************************/
/* Setup one session to be used by all functions called */
mcuxClSession_Descriptor_t sessionDesc;
mcuxClSession_Handle_t session = &sessionDesc;
MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_SESSION(session, MAX_CPUWA_SIZE, MAX_PKCWA_SIZE);
uint32_t pubKeyDesc[MCUXCLKEY_DESCRIPTOR_SIZE_IN_WORDS];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
mcuxClKey_Handle_t pubKey = (mcuxClKey_Handle_t) &pubKeyDesc;
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
/**************************************************************************/
/* Verify with a valid public key */
/**************************************************************************/
MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(ki_pub_status, ki_pub_token, mcuxClKey_init(
/* mcuxClSession_Handle_t session */ session,
/* mcuxClKey_Handle_t key */ pubKey,
/* mcuxClKey_Type_t type */ mcuxClKey_Type_WeierECC_NIST_P256_Pub,
/* const uint8_t * pKeyData */ pubKeyBytes,
/* uint32_t keyDataLength */ MCUXCLECC_WEIERECC_NIST_P256_SIZE_PUBLICKEY)
);
if((MCUX_CSSL_FP_FUNCTION_CALLED(mcuxClKey_init) != ki_pub_token) || (MCUXCLKEY_STATUS_OK != ki_pub_status))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/* Signature Verification with a valid public key */
MCUXCLBUFFER_INIT_RO(buffData, NULL, data, sizeof(data));
MCUXCLBUFFER_INIT_RO(buffSignature, NULL, signature, sizeof(signature));
/* Record critical parameters for additional protection */
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_SESSION")
/* mcuxClSession_Handle_t session: */ session,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
/* mcuxClSignature_Mode_t mode: */ mcuxClSignature_Mode_ECDSA,
/* mcuxCl_InputBuffer_t pIn: */ buffData,
/* uint32_t inSize: */ sizeof(data))
);
if((MCUX_CSSL_FP_FUNCTION_CALLED(mcuxClSignature_verify_recordParam) != rp_token) || (MCUXCLSIGNATURE_STATUS_OK != rp_status))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/* mcuxClSession_Handle_t session: */ session,
/* mcuxClKey_Handle_t key: */ pubKey,
/* mcuxClSignature_Mode_t mode: */ mcuxClSignature_Mode_ECDSA,
/* mcuxCl_InputBuffer_t pIn: */ buffData,
/* uint32_t inSize: */ sizeof(data),
/* mcuxCl_InputBuffer_t pSignature: */ buffSignature,
/* uint32_t signatureSize: */ sizeof(signature))
);
/* Check the token and return status and return accordingly */
if((MCUX_CSSL_FP_FUNCTION_CALLED(mcuxClSignature_verify) == sv_token) && (MCUXCLSIGNATURE_STATUS_OK == sv_status))
{
/* Signature OK scenario */
return MCUXCLEXAMPLE_STATUS_OK;
}
(MCUXCLSIGNATURE_STATUS_NOT_OK == sv_status))
{
/* Signature NOT OK scenario */
return MCUXCLEXAMPLE_STATUS_ERROR;
}
else if(MCUXCLCORE_CLS_ABNORMAL == MCUXCLCORE_GET_CLS(sv_status))
{
/* Error scenario */
/* Perform cleanuponError and release the used resources */
MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(resultCleanup, tokenCleanup, mcuxClSession_cleanupOnError(session));
(MCUXCLSESSION_STATUS_OK != resultCleanup))
{
return MCUXCLEXAMPLE_STATUS_FAILURE;
}
return MCUXCLEXAMPLE_STATUS_ERROR;
}
else
{
/* Fault scenario */
/* The cleanuponError function should not be used here, but instead Power-On-Reset or System Reset must be performed. */
return MCUXCLEXAMPLE_STATUS_ERROR;
}
}
Top-level include file for the mcuxClBuffer component.
Definition of function identifiers for the flow protection mechanism.
Top level header of mcuxClEcc component.
Top-level include file for the mcuxClHash component.
Top-level include file for the mcuxClKey component.
Top-level include file for the mcuxClSession component.
Top-level include file for the mcuxClSignature component.
Provides the API for the CSSL flow protection mechanism.
#define MCUXCLBUFFER_INIT_RO(name, info, ptr, size)
Initialize an input buffer (mcuxCl_InputBuffer_t) with plain CPU handling.
Definition mcuxClBuffer.h:84
static const mcuxClKey_Type_t mcuxClKey_Type_WeierECC_NIST_P256_Pub
Key type pointer for public ECC Weierstrass keys for Weierstrass curve NIST P-256.
Definition mcuxClEcc_KeyTypes.h:453
#define MCUXCLKEY_STATUS_OK
Key operation successful.
Definition mcuxClKey_Constants.h:40
mcuxClKey_Status_t mcuxClKey_init(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClKey_Type_t type, const uint8_t *pKeyData, uint32_t keyDataLength)
Initializes a key handle.
mcuxClKey_Descriptor_t *const mcuxClKey_Handle_t
Key handle type.
Definition mcuxClKey_Types.h:91
mcuxClSession_Status_t mcuxClSession_cleanupOnError(mcuxClSession_Handle_t pSession)
Clean up HW Resources after error case.
#define MCUXCLSESSION_STATUS_OK
Session operation successful.
Definition mcuxClSession_Types.h:39
mcuxClSession_Descriptor_t *const mcuxClSession_Handle_t
Type for mcuxClSession Handle.
Definition mcuxClSession_Types.h:98
mcuxClSignature_Status_t mcuxClSignature_verify(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClSignature_Mode_t mode, mcuxCl_InputBuffer_t pIn, uint32_t inSize, mcuxCl_InputBuffer_t pSignature, uint32_t signatureSize)
One-shot verification function.
mcuxClSignature_Status_t mcuxClSignature_verify_recordParam(mcuxClSession_Handle_t pSession, mcuxClSignature_Mode_t mode, mcuxCl_InputBuffer_t pIn, uint32_t inSize)
Record signature verification parameters for protection.
#define MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(...)
Call a flow protected function and check the protection token.
Definition mcuxCsslFlowProtection.h:623
#define MCUX_CSSL_FP_FUNCTION_CALLED(...)
Expectation of a called function.
Definition mcuxCsslFlowProtection.h:777
#define MCUX_CSSL_FP_FUNCTION_CALL_END(...)
End a function call section started by MCUX_CSSL_FP_FUNCTION_CALL_BEGIN.
Definition mcuxCsslFlowProtection.h:658
static mcuxClSignature_Mode_t mcuxClSignature_Mode_ECDSA
ECDSA Signature mode.
Definition mcuxClEcc_Types.h:211