MCUX CLNS
MCUX Crypto Library Normal Secure
 
Loading...
Searching...
No Matches
File List
Here is a list of all documented files with brief descriptions:
[detail level 1234]
  examples
  platform
 mcuxCl_clns.hCLNS header for component-independent functionality
 mcuxClAead.hTop-level include file for the mcuxClAead component
 mcuxClAead_Constants.hConstants for use with the mcuxClAead component
 mcuxClAead_Functions.hTop-level API of the mcuxClAead component
 mcuxClAead_Types.hType definitions for the mcuxClAead component
 mcuxClAeadModes.h
 mcuxClAeadModes_Modes.hThis file defines the modes for the mcuxClAeadModes component
 mcuxClAes.hTop-level interface header for the mcuxClAes component
 mcuxClAes_Constants.h
 mcuxClAes_KeyTypes.hDefinition of supported key types in mcuxClAes component, see also mcuxClKey component
 mcuxClAes_Types.hType definitions for the mcuxClAes component
 mcuxClBuffer.hProvides the API for the CL buffer types
 mcuxClBuffer_Cfg.hConfiguration of the implementation for the buffer types
 mcuxClBuffer_Constants.hConstants for use with the mcuxClBuffer component
 mcuxClBuffer_Impl.hSelection of the implementation for the buffer types
 mcuxClBuffer_Pointer.hProvides the implementation for the basic C pointer buffer types
 mcuxClCipher.hTop-level include file for the mcuxClCipher component
 mcuxClCipher_Constants.hConstants for use with the mcuxClCipher component
 mcuxClCipher_Functions.hTop-level API of the mcuxClCipher component
 mcuxClCipher_Types.hType definitions for the mcuxClCipher component
 mcuxClCipherModes.h
 mcuxClCipherModes_Modes.hSupported modes for the mcuxClCipher component
 mcuxClCore_Examples.h
 mcuxClCore_FunctionIdentifiers.hDefinition of function identifiers for the flow protection mechanism
 mcuxClCore_Macros.hDefinition of macros
 mcuxClCore_Platform.h
 mcuxClCore_Toolchain.h
 mcuxClCrc.hTop-level include file for the mcuxClCrc component
 mcuxClEcc.hTop level header of mcuxClEcc component
 mcuxClEcc_Constants.hConstant definitions of mcuxClEcc component
 mcuxClEcc_Functions.hTop level APIs of mcuxClEcc component
 mcuxClEcc_KeyTypes.hECC related definitions to be used for key handling mechanisms of the mcuxClKey component
 mcuxClEcc_Types.hType definitions and descriptors of mcuxClEcc component
 mcuxClEls.hTop-level include file for the ELS driver
 mcuxClEls_Aead.hELS header for Authenticated Encryption with Associated Data (AEAD)
 mcuxClEls_Cipher.hELS header for symmetric ciphers
 mcuxClEls_Cmac.hELS header for CMAC support
 mcuxClEls_Common.hELS header for common functionality
 mcuxClEls_Crc.hELS header for Command CRC functionality
 mcuxClEls_Ecc.hELS header for elliptic curve cryptography This header exposes functions that enable using the ELS for elliptic curve cryptography
 mcuxClEls_Hash.hELS header for hashing
 mcuxClEls_Hmac.hELS header for HMAC support
 mcuxClEls_Kdf.hELS header for key derivation
 mcuxClEls_KeyManagement.hELS header for key management
 mcuxClEls_mapping.hHeader providing mapping for legacy function/definition names (with CSS)
 mcuxClEls_Rng.hELS header for random number generation
 mcuxClEls_Types.hELS type header
 mcuxClExample_ELS_Helper.h
 mcuxClExample_ELS_Key_Helper.h
 mcuxClExample_Key_Helper.h
 mcuxClExample_RFC3394_Helper.h
 mcuxClExample_RNG_Helper.h
 mcuxClExample_Session_Helper.h
 mcuxClGlikey.hTop-level include file for the Glikey driver
 mcuxClHash.hTop-level include file for the mcuxClHash component
 mcuxClHash_Constants.hConstants for use with the mcuxClHash component
 mcuxClHash_Functions.hTop-level API of the mcuxClHash component
 mcuxClHash_Types.hType definitions for the mcuxClHash component
 mcuxClHashModes.h
 mcuxClHashModes_Algorithms.hAlgorithm/mode definitions for the mcuxClHashModes component
 mcuxClHashModes_Constants.hConstants for use with the mcuxClHashModes component
 mcuxClHashModes_Functions.h
 mcuxClHmac.h
 mcuxClHmac_Constants.hConstants for the mcuxClHmac component
 mcuxClHmac_Functions.hFunctions for the mcuxClHmac component
 mcuxClHmac_KeyTypes.hDefinition of supported key types in mcuxClHmac component, see also mcuxClKey component
 mcuxClHmac_Modes.hMode descriptors for the mcuxClHmac component
 mcuxClKey.hTop-level include file for the mcuxClKey component
 mcuxClKey_Constants.hConstants for the mcuxClKey component
 mcuxClKey_DerivationAlgorithms.hSupported algorithms for key derivation
 mcuxClKey_DerivationAlgorithms_HKDF.hDeclarations and definitions for the Implementation of RFC5869 Key Derivation
 mcuxClKey_DerivationAlgorithms_NIST_SP800_108.hDeclarations and definitions for the NIST SP800-108 KDF
 mcuxClKey_DerivationAlgorithms_NIST_SP800_56C.hDeclarations and definitions for the NIST SP800-56C KDF
 mcuxClKey_DerivationAlgorithms_PBKDF2.hDeclarations and definitions for the Implementation of PBKDF2 Key Derivation
 mcuxClKey_Functions.hTop-level API of the mcuxClKey component
 mcuxClKey_ProtectionMechanisms.h
 mcuxClKey_Types.hType definitions for the mcuxClKey component
 mcuxClMac.hTop-level include file for the mcuxClMac component
 mcuxClMac_Constants.hConstants and status codes for the mcuxClMac component
 mcuxClMac_Functions.hTop-level API of the mcuxClMac component
 mcuxClMac_Types.hType definitions for the mcuxClMac component
 mcuxClMacModes.h
 mcuxClMacModes_Constants.hConstants for the mcuxClMacModes component
 mcuxClMacModes_Functions.hFunctions for the mcuxClMacModes component
 mcuxClMacModes_Modes.h
 mcuxClMath.hTop level header of mcuxClMath component
 mcuxClMath_Functions.hAPIs of mcuxClMath component
 mcuxClMath_Types.h
 mcuxClMemory.hTop-level include file for the memory operations
 mcuxClMemory_Clear.hMemory header for clear functions
 mcuxClMemory_Constants.hMemory constant header
 mcuxClMemory_Copy.hMemory header for copy functions
 mcuxClMemory_Copy_Reversed.hMemory header for reversed copy functions
 mcuxClMemory_Endianness.hMemory header for endianness support functions
 mcuxClMemory_Set.hMemory header for set function
 mcuxClMemory_Types.hMemory type header
 mcuxClMemory_Xor.hMemory header for xor functions
 mcuxClOscca_FunctionIdentifiers.hDefinition of function identifiers for the flow protection mechanism
 mcuxClOscca_Memory.h: Macros for alignment memory
 mcuxClOscca_PlatformTypes.h: Platform type definitions
 mcuxClOscca_Types.h: Global type definitions
 mcuxClOsccaAeadModes.hTop-level include file for the mcuxClOsccaAeadModes component
 mcuxClOsccaAeadModes_Modes.hSupported modes for the mcuxClOsccaAeadModes component
 mcuxClOsccaCipherModes.hTop-level include file for the constants definitions component
 mcuxClOsccaCipherModes_Constants.hSupported constants for the mcuxClOsccaCipherModes component
 mcuxClOsccaMacModes.h
 mcuxClOsccaMacModes_Constants.hHeader for mac constants
 mcuxClOsccaMacModes_KeyTypes.hDefinition of supported key types in mcuxClOsccaMacModes component
 mcuxClOsccaMacModes_Modes.h
 mcuxClOsccaPkc.hTop level header of mcuxClOsccaPkc component (PKC hardware driver)
 mcuxClOsccaPkc_Functions.hAPIs of mcuxClOsccaPkc component
 mcuxClOsccaPkc_Types.hType definitions of mcuxClOsccaPkc component
 mcuxClOsccaRandomModes.hTop level header of mcuxClOsccaRandomModes component
 mcuxClOsccaRandomModes_Constants.hMode definitions of mcuxClOsccaRandomModes component
 mcuxClOsccaSafo.hTop level header of mcuxClOsccaSafo component (SAFO hardware driver)
 mcuxClOsccaSafo_Constants.hSAFO constant header
 mcuxClOsccaSafo_Functions.h
 mcuxClOsccaSafo_Sfr_Ctrl.h
 mcuxClOsccaSafo_Sfr_RegBank.h
 mcuxClOsccaSafo_Sfr_Status.h
 mcuxClOsccaSafo_SfrAccess.hMacros for abstracting SAFO hardware SFR access
 mcuxClOsccaSafo_Types.hType and associated constant definitions of the mcuxClOsccaSafo component
 mcuxClOsccaSm2.hTop level header of mcuxClOsccaSm2 component
 mcuxClOsccaSm2_Constants.h: Platform related definitions for the OSCCA SM2 component
 mcuxClOsccaSm2_Functions.hTop level APIs of mcuxClOsccaSm2 component
 mcuxClOsccaSm2_KeyTypes.hDefinition of supported key types in mcuxClOsccaSm2 component, see also mcuxClKey component
 mcuxClOsccaSm2_ModeConstants.h: Platform related mode definitions for the OSCCA SM2 component
 mcuxClOsccaSm2_SelfTest.h: Self test function prototype definitions for the OSCCA SM2 component
 mcuxClOsccaSm2_Types.hType definitions of mcuxClOsccaSm2 component
 mcuxClOsccaSm3.hTop-level include file for the mcuxClOsccaSm3 component
 mcuxClOsccaSm3_Algorithms.hAlgorithm/mode definitions for the mcuxClOsccaSm3 component
 mcuxClOsccaSm3_Constants.hConstants for use with the mcuxClOsccaSm3 component
 mcuxClOsccaSm4.hTop level header of mcuxClOsccaSm4 component
 mcuxClOsccaSm4_KeyTypes.hDefinition of supported key types in mcuxClOsccaSm4 component, see also mcuxClKey component
 mcuxClPadding.hTop-level include file for the padding component
 mcuxClPadding_Constants.hConstants definitions for the mcuxClPadding component
 mcuxClPadding_Types.hType definitions for the mcuxClPadding component
 mcuxClPkc.hTop level header of mcuxClPkc component (PKC hardware driver)
 mcuxClPkc_Functions.hAPIs of mcuxClPkc component
 mcuxClPkc_Types.hType definitions of mcuxClPkc component
 mcuxClRandom.hTop level header of mcuxClRandom component
 mcuxClRandom_Constants.hConstant definitions of mcuxClRandom component
 mcuxClRandom_Functions.hTop level APIs of mcuxClRandom component
 mcuxClRandom_Types.hType definitions of mcuxClRandom component
 mcuxClRandomModes.hTop level header of mcuxClRandomModes component
 mcuxClRandomModes_Constants.hMode definitions of mcuxClRandomModes component
 mcuxClRandomModes_Functions_PatchMode.h
 mcuxClRandomModes_Functions_TestMode.h
 mcuxClRsa.hTop-level include file for the mcuxClRsa component
 mcuxClRsa_Constants.hConstant definitions for the mcuxClRsa component
 mcuxClRsa_Functions.hTop-level API of the mcuxClRsa component
 mcuxClRsa_KeyTypes.hDefinition of supported key types in mcuxClRsa component, see also mcuxClKey component
 mcuxClRsa_ModeConstructors.h
 mcuxClRsa_Types.hType definitions for the mcuxClRsa component
 mcuxClSession.hTop-level include file for the mcuxClSession component
 mcuxClSession_Functions.hTop-level API of the mcuxClSession component
 mcuxClSession_Types.hType definitions for the mcuxClSession component
 mcuxClSignature.h
 mcuxClSignature_Constants.h
 mcuxClSignature_Functions.h
 mcuxClSignature_Types.h
 mcuxCsslAnalysis.h
 mcuxCsslCPreProcessor.hThe default implementation is based on standard C preprocessor functionality
 mcuxCsslDataIntegrity.hProvides the API for the CSSL data integrity mechanism
 mcuxCsslDataIntegrity_Cfg.hConfiguration of the implementation for the data integrity mechanism
 mcuxCsslDataIntegrity_Impl.hSelection of the implementation for the data integrity mechanism
 mcuxCsslDataIntegrity_None.hImplementation that disables the CSSL data integrity mechanism
 mcuxCsslFlowProtection.hProvides the API for the CSSL flow protection mechanism
 mcuxCsslFlowProtection_Cfg.hConfiguration of the implementation for the flow protection mechanism
 mcuxCsslFlowProtection_FunctionIdentifiers.hDefinition of function identifiers for the flow protection mechanism
 mcuxCsslFlowProtection_Impl.hSelection of the implementation for the flow protection mechanism
 mcuxCsslFlowProtection_SecureCounter_Common.hCounter based implementation for the flow protection mechanism, for a local security counter
 mcuxCsslFlowProtection_SecureCounter_Local.hCounter based implementation for the flow protection mechanism, for a local security counter
 mcuxCsslMemory.hTop-level include file for the CSSL memory functions
 mcuxCsslMemory_Clear.hHeader file of memory clear function
 mcuxCsslMemory_Compare.hInclude file for constant time memory compare function
 mcuxCsslMemory_Constants.hConstants definitions for the mcuxCsslMemory component
 mcuxCsslMemory_Copy.hInclude file for memory copy function
 mcuxCsslMemory_Set.hHeader file of memory set function
 mcuxCsslMemory_Types.hType definitions for the mcuxCsslMemory component
 mcuxCsslParamIntegrity.hTop-level include file for the parameter integrity protection mechanism
 mcuxCsslSecureCounter.hProvides the API for the CSSL secure counter mechanism
 mcuxCsslSecureCounter_Cfg.hConfiguration of the implementation for the secure counter mechanism
 mcuxCsslSecureCounter_Impl.hSelection of the implementation for the secure counter mechanism
 mcuxCsslSecureCounter_None.hImplementation that disables the CSSL secure counter mechanism
 mcuxCsslSecureCounter_SW_Local.hSW implementation of the CSSL secure counter mechanism (using a local variable)