# User interface
This chapter provides a detailed description of the user interface.
## Start Development wizard
Upon starting MCUXpresso Config Tools, you are automatically welcomed by a startup wizard. With this wizard, you can create a configuration or open an existing one.
**Note:** To skip the wizard on subsequent startups, select the **Always open last configuration** checkbox below the **Open an existing configuration** option. You can also perform the same action by selecting the **Automatically open previously used configuration** checkbox in **Preferences**.
```{eval-rst}
.. figure:: _images/start_development_wizard.png
:scale: 30%
:align: center
**Start development wizard**
```
**Note:** The content of this wizard is similar to the wizard that you open by selecting **File > New** in the **Menu bar**.
## Creating, saving, and opening a configuration
In this context, configuration stands for common tools settings stored in an MEX \(Microcontrollers Export Configuration\)file. This file contains the settings of all available tools and can be used in both web and desktop versions.
The folder with the saved MEX file must contain exactly one project file to be able to parse the toolchain project. The file type depends on the toolchain of the project and can be one of the following:
### Table Supported toolchain project files
```{table} Supported toolchain project files
:name: supported-toolchain-project-files
|Toolchain|Project file|
|---------|------------|
|IAR Embedded Workbench|EWP|
|Keil MDK uVision|UVPROJX|
|ARM GCC|CMakeLists.txt|
|CodeWarrior with SDK|.cproject|
|Open-CMSIS csolution|\*.cbuild-gen-idx.yml|
|SDK West|project\_info.json|
```
### Creating a new configuration
You can create a configuration from the **Start development** wizard or by selecting **File > New** from the **Menu bar**.
If you start creating your development for any NXP board or kit, we recommended you start with an MCUXpresso SDK example to create a configuration for a board or a kit. Such a configuration contains board-specific settings. If you select a processor, the configuration will be empty.
After the new configuration is created, you can continue by importing an existing configuration from an MEX file. It is useful if you already have a configuration available or if you want to reuse a previous configuration. To import an existing configuration from an MEX file, select **File > Import... > Import configuration \(\*.mex\)** from the **Menu bar**.
#### Cloning an SDK example
You can create a configuration by cloning an SDK example project for IAR Embedded Workbench, Keil μVision, CodeWarrior Development Studio, and/or GCC ARM Embedded \(command line\). The resulting project contains all source files and libraries to build the project and can be easily customized, shared, or put under a control version system.
**Note:** The creation \(cloning\) of the projects based on the SDK examples will no longer be supported in the future releases of the MCUXpresso Config Tools. Instead, use use the MCUXpresso SDK CMake, Kconfig-based build. For detailed documentation, see the SDK Build And Configuration System documentation.
SDK example cloning is supported for MCUXpresso SDK 2.2 and higher.
**Note:** To be able to clone an SDK example or create a "hello\_world" project, you must first download an SDK package. For more information about SDK packages offered by NXP Semiconductors, refer to the [MCUXpresso Software Development Kit](https://www.nxp.com/support/developer-resources/software-development-tools/mcuxpresso-software-and-tools/mcuxpresso-software-development-kit-sdk:MCUXpresso-SDK).
**Note:** If the server is unavailable, and device data is not cached, creating the project fails.
```{eval-rst}
.. figure:: _images/start_dev_project_corrected.png
:scale: 30%
:align: center
**Cloning SDK**
```
To clone an SDK example, do the following:
1. In the **Start development** wizard, select **Create a new configuration based on an SDK example or a "hello world" project**. Alternatively, in the **Menu bar**, select **File > New**.
2. Click **Next**.
3. Specify the path to your locally saved SDK package.
4. Choose the toolchain that you want to create the project for.
5. Choose the SDK example that you want to clone.
6. Specify a base project directory to save your project to.
7. Specify the project name.
8. Click **Finish**.
You can also create a basic, minimally customized "hello\_world" project without having to select an SDK example from the package. To create a "hello\_world" project, do the following:
1. In the **Start development** wizard, select **Create a new configuration based on an SDK example or a "hello world" project**. Alternatively, in the **Menu bar**, select **File > New**.
2. Click **Next**.
3. Specify the path to your locally saved SDK package.
4. Choose the toolchain that you want to create the project for.
5. Select **Create "hello\_world"**.
6. Specify a base project directory to save your project to.
7. Specify the project name.
8. Click **Finish**.
The Config Tools Overview window shows the details of the configuration and supported tools. Now, select a tool by clicking its icon.
#### Creating a new toolchain configuration
You can create a configuration for an existing toolchain project. Once done, configuration files associated with the project are updated directly.
MCUXpresso Config Tools currently supports the following toolchains:
- IAR Embedded Workbench
- Keil MDK uVision
- Arm GCC
- CodeWarrior with SDK
- SDK West
**Note:** For proper functionality of Config Tools, it is required that the toolchain project originates from the SDK package or has been created using the cloning feature of Config Tools.
To create a configuration based on an existing IDE/Toolchain project, do the following:
1. In the **Start development** wizard, select the **Create a new configuration based on an existing IDE/Toolchain project**. Alternatively, in the **Menu bar**, select **File > New**.
2. Click **Browse**.
3. Select the project file and confirm by clicking **OK**.
4. Click **Finish**.
#### Creating a new configuration for SDK West
You can create a configuration, for new format of SDK project \([https://mcuxpresso.nxp.com/mcuxsdk](https://mcuxpresso.nxp.com/mcuxsdk)\) that uses the West tool.
If you are also using Visual Studio Code, you can open Config Tools from there via the context menu for the project. This also opens or creates a new configuration if it does not exist. Otherwise, it is possible to handle it manually using the following steps:
1. Before using config tools, run the west command to get the project information for Config tools from the SDK project files, for example:
```
west cfg_project_info -b lpcxpresso55s69 ...mcuxsdk/examples/demo_apps/hello_world/ -Dcore_id=cm33_core0
```
This results in the creation of the project information json file that is searched by the config tools when the configuration is created. The parameters of the command should match the build parameters that will be used for the project.
2. In the **Start development** wizard, select **Create a new configuration** based on the existing IDE/Toolchain project, and select the created "cfg\_tools" subfolder as a project folder \(for example: ...`mcuxsdk/examples/demo_apps/hello_world/cfg_tools/`\).
#### Creating a new configuration for Zephyr RTOS
You can create a configuration, that generates .dtsi file with pin control that is possible to include in the board device tree. There will be offered only processors/boards
After the configuration, move the generated file to the proper location in your Zephyr board, application folder, or repository. Consult [Zephyr RTOS documentation](https://docs.zephyrproject.org/latest/hardware/pinctrl/index.html) for the appropriate placement and usage of the Pin Control file.
In the context of Zephyr RTOS, only the Pins tool is supported allowing pin routing and configuration.
You can create a configuration that generates a .dtsi file with pin control that can be included in the board device tree. Only processors and boards compatible with the Zephyr \([https://www.nxp.com/zephyr](https://www.nxp.com/zephyr)\) will be offered as the SDK version.
1. In the **Start development** wizard, select **Create a new standalone configuration for Zephyr RTOS**. Alternatively, in the **Menu bar**, select **File > New**.
2. Click **Next**.
3. Select the processor, board, or kit from the list.
**Note:** When working offline, only locally stored options will be available. For further details, refer to the Working Offline section.
4. Name your configuration. Optionally, select the processor package, core, and SDK version.
5. Click **Finish**.
##### Using the generated files
There are some additional manual steps needed to integrate the generated files:
1. After the configuration, write the files to disk using the **Update Code** command or via the **Export** command.
2. Move the generated device tree \(`.dtsi`\) file to the proper location in your Zephyr board, application folder, or repository. If you have a custom hardware, it is a common practice to create a custom board in the Zephyr RTOS rather than modifying standard board files that are shared by many projects. Consult [Zephyr RTOS documentation](https://docs.zephyrproject.org/latest/hardware/pinctrl/index.html) for details on how to work with pin control and the steps for creation of the custom board.
**Note:** : Alternatively you can leverage content of the .dtsi file for creation of the device tree overlay file for your application.
3. In case features not supported by Zephyr RTOS are used, the Pins tools provides `pin_mux.c/h` files. It is necessary to add `pins.c/h` to your `cmake` file so they are part of the build and call the generated functions in your code.
##### Limitations
The pin configuration and routing cannot be restored from the generated `.dtsi` file because there is no import functionality for this format. Keep the original `.mex` file for further regeneration of the file\(s\).
#### Creating a new standalone configuration
You can create a configuration that is not part of any toolchain project.
You can later include this configuration in a project by saving the configuration \(MEX\) file in the toolchain project folder.
```{eval-rst}
.. figure:: _images/create_a_new_configuration_25.09.png
:scale: 40%
:align: center
**Creating a new configuration**
```
To create a standalone configuration, do the following:
1. In the **Start development** wizard select **Create a new standalone configuration for processor, board, or kit**. Alternatively, in the **Menu bar**, select **File > New**.
2. Click **Next**.
3. Select the processor, board, or kit from the list.
**Note:** If you are working offline, you will only see locally saved options. For more information, see the [Working offline](./advanced_features.md#working-offline) section.
4. Name your configuration. Optionally, you can select processor package, core, and SDK version.
5. Click **Finish**.
### Saving a configuration
To save your configuration for future use, select **File > Save** from the **Menu bar**.
To save a back-up of your configuration, do the following:
1. In the **Menu bar**, select **File > Save Copy As**.
2. In the dialog, specify the name and destination of the configuration.
3. Click **Save**.
#### Opening an existing configuration
To open an existing configuration, do the following:
1. In the **Start development** wizard, select **Open an existing configuration**. Alternatively, in the **Menu bar**, select **File > Open**.
2. Click **Browse** to navigate to your configuration file.
3. Select the configuration file and click **Open**.
4. Optionally, select **Always open last configuration** to skip the **Start development** wizard and load the last-saved configuration by default.
### User templates
You can export and store the current configuration as a user template for later use as a reference configuration file.
```{eval-rst}
.. figure:: _images/export_configuration_as_template.png
:scale: 60%
:align: center
**Export template**
```
The exported template is available in the **New Configuration** wizard and can be used to create a configuration. You can also define custom labels for pins or identifiers prefixes for `#define` in the generated code. You can export the configuration by selecting, in the **Menu bar**, **File > Export > Tools Configuration > Export Configuration as Template**.
```{eval-rst}
.. figure:: _images/newtemplate_desktop.png
:scale: 40%
:align: center
**Create a new configuration from the template**
```
**Note:** The templates are stored in at the following location on your local hard disk: `{$user}/.nxp/{tools_folder}/{version}/templates`.
### Importing sources
You can import source code files to use as a basis for further configuration.
**Note:** You can import only C or DTSI files containing valid YAML configuration blocks generated by the Config Tools. The configuration is reconstructed from the YAML block and the rest of the imported file is ignored.
To import source code files, do the following:
1. In the **Menu bar**, select **File > Import...**.
2. From the list, select **MCUXpresso Config Tools > Import Source**.
```{eval-rst}
.. figure:: _images/import_wizard.png
:scale: 60%
:align: center
**Import Source wizard**
```
3. Click **Next**.
4. On the next page, click **Browse** to specify the location of the source file.
5. Select the source file that you wish to import and click **Open**.
6. On the next page, select which functional groups to import \(based on tools\) by selecting the checkbox in the left column.
7. Define how to import the functional groups by selecting one of the two available options in the dropdown menu in the right column:
- **Rename** – All files are merged into the current configuration. It imports all the functions only. If the imported function has the same name as an existing one, it is automatically renamed to the indexed one. For example, if `BOARD_InitPins` exists in the configuration then the imported function is renamed to `BOARD_InitPins1`.
- **Overwrite** – All files are merged into the current configuration. It imports all the functions only. If the imported function has the same name as an existing one, then the existing one is replaced with the imported one.
8. Click **Finish**.
#### Importing configuration
To import an existing configuration from an MEX file, do the following:
1. In the **Menu bar**, select **File > Import...>**.
2. In the **Import** wizard, select **MCUXpresso Config Tools > Import configuration \(\*.mex\)**.
3. Click **Next**.
4. On the next page, click **Browse** to specify the location of the registers file.
5. Select the MEX file that you wish to import and click **Open**.
6. On the next page, select which functional groups to import \(based on tools\) by selecting the checkbox in the left column.
7. Define how to import the functional groups by selecting one of the two available options in the dropdown menu in the right column:
- **Rename** – All files are merged into the current configuration. It imports all the functions only. If the imported function has the same name as an existing one, it is automatically renamed to the indexed one. For example, if `BOARD_InitPins` exists in the configuration then the imported function is renamed to `BOARD_InitPins1`.
- **Overwrite** – All files are merged into the current configuration. It imports all the functions only. If the imported function has the same name as an existing one, then the existing one is replaced with the imported one.
8. Click **Finish**.
```{eval-rst}
.. figure:: _images/import_configuration.png
:scale: 60%
:align: center
**Import configuration**
```
#### Importing Board/Kit Configuration
Use import settings from default board/kit templates provided within CFG tools data for further configuration.
To import a board/kit configuration, do the following:
1. In the **Menu bar**, select **File > Import...>**.
2. In the **Import** wizard, select **MCUXpresso Config Tools > Import Board/Kit Configuration**.
3. Click **Next**.
4. On the next page, select the board/kit variant from the dropdown menu.
5. Select which functional groups to import \(based on tools\) by selecting the checkbox in the left column.
6. Define how to import the functional groups by selecting one of the two available options in the dropdown menu in the right column:
- **Rename** – All files are merged into the current configuration. It imports all the functions only. If the imported function has the same name as an existing one, it is automatically renamed to the indexed one. For example, if BOARD\_InitPins exists in the configuration then the imported function is renamed to BOARD\_InitPins1.
- **Overwrite** – All files are merged into the current configuration. It imports all the functions only. If the imported function has the same name as an existing one, then the existing one is replaced with the imported one.
7. Click **Finish**.
#### Importing registers
You can import a register configuration from a processor memory dump.
**Note:** Currently, register configuration can be imported into the Clocks tool only.
**Note:** A processor memory-dump file in the CSV or S19 format is required for importing register configuration.
```{eval-rst}
.. figure:: _images/import_registers.png
:scale: 60%
:align: center
**Import registers**
```
To import register configuration, do the following:
1. In the **Menu bar**, select **File > Import…**. Alternatively, click the **Import Registers Configuration** button in the **Registers** view, or drag-and-drop the memory dump file anywhere in the **Registers** view area.
```{eval-rst}
.. figure:: _images/import_registers_configuration.png
:scale: 60%
:align: center
**Import registers configuration**
```
2. In the **Import** wizard, select **MCUXpresso Config Tools > Import Registers**.
3. Click **Next**.
4. On the next page, click **Browse** to specify the location of the registers configuration.
5. Select the registers file you wish to import, and click **OK**.
6. By default, the imported register configuration will overwrite the existing functional group. If you want a new functional group to be created instead, select the **Create new functional group** option button, and specify the functional group name.
7. Click **Finish**.
**Note:** All registers are imported from the dump file regardless of their relevance to clock configuration, therefore, the list can contain registers not needed by the Clocks tool.
#### Restoring configuration from source code
All Config tools have a possibility of restoring a configuration from the source code. The generated code below contains information about the Clocks tool settings that are used in the tool \(block within a comment in YAML format\).
The following is an example of the settings information in the generated source code.
```{eval-rst}
.. figure:: _images/clk_09_src_import.png
:scale: 60%
:align: center
**Setting Information in the source code**
```
If this information is not corrupted, it is possible to reimport the clock settings into the tool using the following steps.
1. In the **Menu bar**, select **File > Import…**.
2. From the list, select **MCUXpresso Config Tools > Import Source Files**.
3. Click **Next**.
4. Click **Browse**.
5. Navigate and select the source file previously produced by one of the Config tools \(for example, *clock\_config.c*\).
6. If the settings parse successfully, the clock configurations are added into the current global configuration.
## Menu bar
The **Menu bar** contains six menus: **File, Edit, Tools, Views, Help,** and a **tool-specific menu**.
The **File** menu contains file management items.
### Table File menu
```{table} File menu
:name: file-menu
|Menu item|Description|
|---------|-----------|
|**New...**|Create a configuration. For more information, see the [Configuration](#creating-saving-and-opening-a-configuration) section.|
|**Open**|Open a configuration from an MEX file.|
|**Save**|Save the current configuration.|
|**Save Copy As...**|Create a backup copy of the current configuration.|
|**Switch processor**|Switch to a different processor. For more information, see the [Switching processor](./advanced_features.md#switching-the-processor) section.|
|**Switch package**|Switch to a different processor package. For more information, see the [Switching processor](./advanced_features.md#switching-the-processor) section.|
|**Select Core**|Select a processor core for further configuration.|
|**Data Manager**|Manage local data. For more information, see the [Managing data and working offline](./advanced_features.md#managing-data-and-working-offline) section.|
|**Import...**|Import settings from source files. For more information, see the [Advanced Features](./advanced_features.md) section.|
|**Export...**|Export source files and other tool information. For more information, see the [Advanced Features](./advanced_features.md) section.|
|**Exit**|Exit the application. If there are any unsaved changes, you are prompted to save the changes.|
```
### Table Edit menu
The **Edit** menu contains basic editing actions and items modifying the appearance and behavior of the whole framework.
```{table} Edit menu
:name: edit-menu
|Menu item|Description|
|---------|-----------|
|**Open Update Code Dialog**|Update code after configuration change. For more information, see the [Update code](#update-code) section.|
|**Undo \(...\)**|Cancel a previous action. The action to be undone is always appended.|
|**Redo \(...\)**|Cancel a previous undo action. The action to be redone is always appended.|
|**Copy**|Copy the selected text to the clipboard.|
|**Select All**|Select the whole text in the current field/view.|
|**Call from default initialization function**|Set the currently selected functional group to be called from the default initialization function.|
|**Functional Group Properties**|Edit functional group properties.|
|**Preferences**|Edit preferences. For more information, see the [Preferences](#preferences) section.|
|**Configuration Preferences**|Edit configuration preferences. For more information, see the [Configuration Preferences](#configuration-preferences) section.|
```
### Table Tool-specific menu
The **Tools** menu lists all the tools available in the tools framework. Use this menu to switch between the tools.
The **Tool-specific** menu contains items tailor-made for individual tools. Only items relevant to the currently active tool are displayed. The menu name copies the name of the currently active tool.
```{table} Tool-specific menu
:name: tool-specific-menu
|Item|Description|
|----|-----------|
|**Functional Groups**|Open the Functional group properties window.|
|**Refresh**|Refresh both the generated code and the whole GUI.|
|**Reset to Board Defaults**|Reset the configuration of the Board/Kit defaults.|
|**Reset to Processor Defaults**|Reset the configuration of the processor's defaults.|
|**Automatic Routing** \(Pins\)|Attempt to resolve routing issues. Opens the **Automatic Routing** dialog, which displays the routing issues that have been resolved and the ones that require manual correction.|
|**Apply Expansion Board** \(Pins\)|Apply an expansion board to an already created expansion header|
|**Create Default Routing** \(Pins\)|Open a dialog for the creation of a new functional group containing the after-reset state of pins and internal signals.|
|**Unlock All Settings** \(Clocks\)|Unlock all currently active locks.|
|**Unlock Settings on the Active Path** \(Clocks\)|Unlock all settings on the selected path.|
|**Global Settings** \(Peripherals\)|Open a tab aggregating the global settings of all configuration sets.|
|**Component use case library** \(Peripherals\)|Open the component use the case manager dialog.|
|**Customize initialization order** \(Peripherals\)|Open a dialog for customization of peripheral initialization order.|
|**Resolve duplicate names error** \(Peripherals\)|Resolve problems with duplicate names of multiple component instances by renaming all conflicted component instances to usable automatic names.|
|**Clear All Commands** \(Device Configuration\)|Remove all entered commands.|
|**Config Tools Snippets** \(Peripherals\)|Open the Config Tools Snippets view.|
|**Migrate to other component versions** \(Peripherals\)|Launch the dialog allowing to migrate settings to other versions of SDK components.|
```
### Table Help menu
The **Views** menu contains a tool-specific list of available views. Select a view from the list to open it. Select an already opened view to highlight it. Choose **Reset views** to reset the current tool perspective to its default state. The **Help** menu contains assistance and general information-related items.
```{table} Help menu
:name: help-menu
|Item|Description|
|----|-----------|
|**Contents**|Display the User Guide.|
|**Quick Start guide**|Open a PDF file of the Quick Start guide.|
|**Release Notes**|Display release notes of the installed version.|
|**Community**|Display web pages of the product-related community forums.|
|**Processor Information**|Display web pages containing information about the currently used processor.|
|**Kit/Board Information**|Display web pages containing information about the currently used board or kit.|
|**Open SDK API**|Display documentation of the relevant SDK API.|
|**Check for updates**|Check for a newer version of the product. If a new version is available, you are prompted to confirm and perform the update|
|**Open Cheat Sheet**|Display a cheat sheet to help with using the tools. You can also load a cheat sheet from a file, or from a URL.|
|**About**|Display general product information.|
```
## Toolbar
The toolbar is on the top of the window and includes buttons/menus of frequently used actions common to all tools. See the following sections for more information.
### Table Toolbar
```{table} Toolbar
:name: toolbar
|Item|Description|
|----|-----------|
|**Config Tools Overview**|Open the **Overview** dialog with information about currently used tools.|
|**Show Problems View**|Open the **Problems** view.|
|**Update Code**|Open the update dialog allowing you to update generated peripheral initialization code directly within the specified toolchain project.|
|**Generate Code**|Regenerate source code when the "Enable Code Preview" preference is disabled.|
|**Functional group selection**|Select a functional group. A functional group in the Peripherals tool represents a group of peripherals that are initialized as a group. The tool generates a C function for each function group that contains the initialization code.|
|**Call from default initialization**|Set the current functional group to be initialized by the default initialization function.|
|**Functional group properties**|Open the **Functional group properties** dialog to modify name and other properties of the function group.|
|**Tool selection**|Display icons of individual tools. Use them to switch between tools.|
|**Undo/Redo**|Undo/Redo last action.|
```
In addition, the toolbar may contain additional items depending on the selected tool. See the chapters dedicated to individual tools for more information.
### Config tools overview button
Click the **Config Tools Overview** button to open **Config Tools Overview** and inspect information about the configuration, hardware, and project. For more information, see the [Config Tools Overview](#config-tools-overview) section.
### Show problems view
Click the **Show Problems View** to open/highlight the **Problems view** and inspect any errors in your configuration. See [Problems view](#problems-view) for more information.
Button color depends on the issue type. Red indicates the presence of at least one error, yellow indicates the presence of at least one warning.
### Update code
To update the generated code in the related toolchain project, click the **Update Code** button. In the window, select the tools or files you want to update. If the file is updated automatically, the button is filled with a black square. The reason is displayed in the tooltip.
**Note**: For multicore projects only the files that are related to the currently selected active core are updated by this command. To get files for other core(s), the **export** command needs to be used instead.
The project information shows the Project name and path or the path to the mex folder, when the configuration is without a project.
```{eval-rst}
.. figure:: _images/updatefiles.png
:scale: 60%
:align: center
**Update Files window**
```
To inspect the code difference between the versions, click the **change** link.
```{eval-rst}
.. figure:: _images/showdiff.png
:scale: 60%
:align: center
**Show differences**
```
To update the project without opening the **Update Files** dialog, deselect the **Always show details before Update Code** checkbox.
To access the **Update Code** dialog from the **Update Code** dropdown menu, select **Open Update Code Dialog**.
```{eval-rst}
.. figure:: _images/updatecode.png
:scale: 60%
:align: center
**Update Code dropdown menu**
```
**Note:** The generated code is always overwritten.
**Note:** Before the current file is overwritten, it is copied with a BAK extension.
The **Update Code** action is enabled under the following conditions:
- MEX configuration file is saved locally
- If the MEX configuration is saved in a toolchain project, the processor selected in the tool matches with the processor selected in the toolchain project
- Core is selected \(for multicore processors\)
### Functional groups
Every **Pins/Clocks/Peripherals/TEE** configuration can contain several functional groups.
These groups represent functions that will be generated into the source code. Use the dropdown menu to switch between functional groups and configure them.
```{eval-rst}
.. figure:: _images/mcux7fungus.png
:scale: 60%
:align: center
**Functional groups**
```
You can use two additional buttons to further configure functional groups:
#### Table Functional Groups
```{table} Functional Groups
:name: functional-groups
|Icon|Description|
|----|-----------|
|!(/_images/n_toolbar_init_button.png)|Toggle "Called from default initialization function" feature \(in source code\)|
|!(/_images/n_toolbar_properties_button.png)|Opens the **Functional group properties** window|
```
**Note:** Red/orange background indicates errors/warnings in the configuration.
#### Functional group properties
In the **Functional Group Properties** window, you can configure several options for functions and code generation. Each setting is applicable for the selected function. You can specify the generated function name, select the core \(for multicore processors only\) that is affecting the generated source code, or write a function description \(this description is generated in the C file\). You can also add, copy, and remove functional groups as needed.
Aside from name and description, you can choose to set parameters for selected functional groups.
Functional group properties are specific for individual Config Tools:
Pins tool:
- **Set custom \#define prefix**- If this property is set, the specific custom prefix is used for macros generated into the `pin_mux.h.` Otherwise the name of the functional group is used as the prefix.
- **Prefix** - The custom prefix string. If it is empty, no prefix is used.
- **Clocks gate enable** - If this property is enabled, the clock gate is enabled in the generated code. The clock gate is needed for access to the peripherals, so have it enabled elsewhere.
- **Core** \(for multicore processors only\) - Selects the core that is used for executing this function.
- **Full pins initialization** - If this property is set, all features of the pins are fully initialized in the generated function even if matches the after-reset state of the processor. If it is not set, values "Not specified" or "No init" can be selected.
- **De-initialization function** - If this feature is set, an additional function that sets all pins and peripheral signals in this functional group to their after-reset state is generated. The new function has a suffix `_deinit` by default.
- **Set custom de-initialization function name**- Allows specifying a user-defined name of the de-initialization function.
Clocks tool:
- **Set custom \#define prefix** - If this property is set, the custom prefix is used for macros define in `clock_config.h.` Otherwise the name of the functional group is used as the prefix.
- **Prefix** - The custom prefix string. If it is empty, no prefix is used.
- **Other settings** - The processor-specific settings are specific for each processor. See the tooltips for details.
Peripherals tool:
- **Prefix** - It is used for identifiers, constants, and functions related to the functional group that is used in generated code. If it is not specified, no prefix is used.
TEE tool:
- **Set custom \#define prefix** - If this property is checked, the custom prefix is used for macros define in the generated code. Otherwise, the name of the functional group is used as the prefix.
```{eval-rst}
.. figure:: _images/fig16_new.png
:scale: 60%
:align: center
**Functional group properties for the Pins tool**
```
```{eval-rst}
.. figure:: _images/functional_group_properties_for_clocks.png
:scale: 60%
:align: center
**Functional group properties for the Clocks tool**
```
```{eval-rst}
.. figure:: _images/functional_group_properties_peripherals.png
:scale: 60%
:align: center
**Functional group properties for Peripherals Tool**
```
### Undo/Redo actions
You can reverse your actions by using the Undo/Redo buttons available in the **Toolbar**. You can also perform these actions from the **Edit** menu in the **Menu bar**.
#### Table Undo/Redo actions
```{table} Undo/Redo actions
:name: undo-redo-actions
|Icon|Description|
|----|-----------|
|!(/_images/undo_icon.png)|Cancels the previous action|
|!(/_images/redo_icon.png)|Cancels the previous undo action|
```
### Selecting the tools
Buttons on the extreme right-hand side of the toolbar represent available tools. Click the icons to quickly navigate between Pins, Clocks, Peripherals, Device Configuration, and TEE tools.
## Status bar
The status bar is visible at the bottom part of the GUI. The status bar indicates the error and warning state of the currently selected functional group.
## Preferences
To configure preferences in the **Preferences** dialog, select **Edit > Preferences** from the **Menu bar**.
**Note:** You can restore settings to default by selecting **Restore Defaults** in the lower right corner of the dialog.
```{eval-rst}
.. figure:: _images/preferences.png
:scale: 60%
:align: center
**Preferences**
```
Several settings are available.
### Table Preferences
```{table} Preferences
:name: preferences
|Item|Description|
|----|-----------|
|**Line ending style**|Select between **Windows \(CR + LF\)**, **Linux/Mac \(LF\)**, or **Default \(based on host\)**.|
|**Generate files read-only**|Prevent modifying the source files unintentionally. Generated source files are marked as read-only.|
|**Always overwrite files without asking**|Update existing files automatically, without prompting.|
|**Always show details before Update Code**|Review changes before the project is updated.|
|**Undo history size**|Enter the maximum number of steps that can be undone. Enter 0 to disable.|
|**Proxy connection**|- **Direct** – Connect directly and avoid a proxy connection.
- **Native** – Use system proxy configuration for network connection.
**Note:** The proxy settings are copied from operating system settings. In case of error, you can specify proxy information in the tools.ini file, located in the <install\_dir>/bin/ folder. Make sure that the file contains the following lines:
- Djava.net.useSystemProxies=true \(already present by default\)
- Dhttp.proxyHost=<somecompany.proxy.net>
- Dhttp.proxyPort=80
**Note:** Authentication is not supported.|
|**Work Offline**|Disable both the connection to NXP cloud and the download of processor/board/kit data.|
|**Processor data update**|Select from the following options:- **Auto Update** – Update the processor data automatically.
- **Manual** – Update processor data after confirmation.
- **Disabled** – Disable processor data update.|
|**Check for application updates**|Check for application updates on a weekly basis|
|**Show pin label & identifier table columns \(Pins Tool\)**|Select to show the pin label and the label identifier in the relevant views.|
|**Require Identifier for Pins \(Pins Tool\)**|Controls generation of pins "Identifier" related warnings. With this preference enabled, warnings will be generated for bidirectional signals that have no Identifier set.|
|**Show Overview window on opening configuration for the first time**|Open the Overview dialog on opening the configuration for the first time.|
|**Help us to improve the tool**|Send device-configuration and tool-use information to NXP. Sending this information to NXP helps fix issues and improve the tools|
|**Automatically load last configuration on startup**|Avoid the startup window and load the last used configuration instead.|
|**Component template folder** \(**Peripherals Tool**\)|The path to the folder with component templates. Keep empty to use the default path. The default path is to the folder component\_templates in the data of the Config tools.|
|**Allow component migrations** \(**Peripherals Tool**\)|When a configuration associated with a toolchain project is open, the peripheral tool automatically checks if the configuration components match the project and suggests a migration if they are not.|
|**Show internal IDs in Peripherals tool**|When checked, the tooltips in the Peripherals tool will contain internal identifications.|
|**Enable animations**|Enables animations in the user interface, such as smoother scrolling or opening a drop-down menu.|
```
### Appearance
In the **Appearance** window, you can configure the look and feel of the user interface.
```{eval-rst}
.. figure:: _images/appearance.png
:scale: 60%
:align: center
**Appearance**
```
The following options are available:
- **Enable theming**
- **Theme**
- **Color and Font Theme**
- **Use round tabs**
- **Use mixed fonts and colors for labels**
- **Show most recently used tabs**
Also, you can select the **Colors and Fonts** subwindow to further specify the appearance of interface elements.
```{eval-rst}
.. figure:: _images/colors_and_fonts.png
:scale: 60%
:align: center
**Colors and Fonts**
```
## Configuration preferences
In the **Configuration preferences** window, you can set your preferences for to the configuration storage file \(MEX\).
To configure the preferences related to the configuration, select **Edit > Configuration Preferences** from the **Menu bar**.
```{eval-rst}
.. figure:: _images/configuration_preferences_new_001.png
:scale: 60%
:align: center
**Configuration Preferences**
```
Several preferences are available.
### Table Configuration Preferences
```{table} Configuration Preferences
:name: configuration-preferences
|Item|Description|
|----|-----------|
|**Validate boot init only**|Validate tools' dependencies only against the 'boot init' function group. When selected, dependencies from all functional groups of all tools must be satisfied in the functional groups marked for default initialization. Clearing this option hides warnings in case the user is using complex scenarios with alternating functional groups within the application code.|
|**Generate YAML**|Generate YAML into C source files.|
|**Custom toolchain project link**|Set the path to the toolchain project folder, otherwise the default path in the same folder as the configuration is used. An absolute path or a relative path to a saved configuration \(MEX\) can be used.
Only for standalone Config Tools.|
|**Custom source file copyright header**|Add a custom copyright header to generated source files that do not already contain copyright.|
|**Generate defines of clock registers**|This feature is disabled by default \(**Edit->Configuration Preferences**\). The new `registers.h` file with registers defines is generated in the **Code Preview** tab. The custom prefix can be defined in the [Functional group properties](#functional-group-properties).|
|**Generate code only for registers that are different from the after-reset state**|Generate code only for registers that are different from the after-reset state. For projects created in earlier MCUXpresso versions, this option is selected by default.|
|**Output path overrides**|Rules that are used to override the path of the output files are generated by the tools. They are applied in the Update code and Exports commands. A special dialog allows editing. For more information, see [Output path overrides](./advanced_features.md#output-path-overrides).|
|**Enable Code Preview**|Controls how the code is generated. When this preference is enabled, code generation is performed automatically after every change in the configuration and the Code Preview is updated accordingly. When this preference is disabled, code generation is stopped, a warning message is displayed in the **Code Preview** window, and the action can be manually triggered by using one of the available options:
- By pressing the "generate code" link highlighted in the warning message from the Code Preview window.
- By pressing the **Update Code** button in the toolbar, where code update is preceded by code generation.|
```
**Warning:** When the source does not contain YAML code, it can't be imported.
## Problems view
The **Problems** view displays issues in individual tools and in the interdependencies between the tools.
```{eval-rst}
.. figure:: _images/problemsview.png
:scale: 60%
:align: center
**Problems view**
```
To open the **Problems** view, click the **Show Problems view** button in the **Toolbar**, or select **Views > Problems** from the **Menu bar**.
The **Problems** table contains the following information:
### Table Problems view
```{table} Problems view
:name: problems-view
|Item|Description|
|----|-----------|
|**Level**|Severity of the problem: Information, Warning, or Error.|
|**Resource**|Resource related to the problem, such as the signal name, the clock signal.|
|**Issue**|Description of the problem.|
|**Origin**|Information on the dependency source.|
|**Target**|Tool that handles the dependency and its resolution.|
|**Type**|Type of the problem. It is either the validation checking dependencies between tools, or a single tool issue.|
```
Every issue comes with a context menu accessible by right-clicking the table row. Use this menu to access information about the problem or to apply a quick fix where applicable. You can also copy the rows for later use by right-clicking the row and selecting **Copy** or by using the **Ctrl+C** shortcut. You can use the **Ctrl+left-click** shortcut to add additional rows to the selection.
**Note:** A quick fix is only available for problems highlighted with the "light bulb" icon.
Filter buttons are available on the right side of the **Problems** view ribbon.
#### Table Filter buttons
```{table} Filter buttons
:name: filter-buttons
|Button|Description|
|------|-----------|
|!(/_images/n_problems_filter_boot.png)|Enables the **Validate boot init only** preference. See the [Configuration preferences](#configuration-preferences) section for details.|
|!(/_images/n_problems_filter_tool.png)|Filters messages in the **Problems** view. If selected, only problems for the active tool are displayed. See the [Configuration preferences](#configuration-preferences) section for details.|
```
## Registers view
The **Registers** view lists the registers handled by the tool models. You can see the state of the processor registers that correspond to the current configuration settings and also the state that is in the registers by default after the reset. The values of the registers are displayed in the hexadecimal and binary form. If the value of the register \(or bit\) is not defined, an interrogation mark "?" is displayed instead of the value.
```{eval-rst}
.. figure:: _images/registers_view_from_the_pins_general.png
:scale: 60%
:align: center
**Registers view**
```
The **Registers view** contains several items.
### Table Registers
```{table} Registers
:name: registers
|Item|Description|
|----|-----------|
|**Peripheral filter** drop-down list|List the registers only for the selected peripheral. Select **all** to list registers for all the peripherals.|
|**Show modified registers only** checkbox|Hide the registers that are left in their after-reset state or are not configured.|
|**Text filter**|Filter content by text.|
|**Import/Export registers**|Import/Export registers from/to CSV \(Import is available only for the Clocks tool\)|
```
The following table lists the color highlighting styles used in the **Registers** view.
### Table Color codes
```{table} Color codes
:name: color-codes
|Color|Description|
|-----|-----------|
|Yellow background|Indicates that the bitfield has been affected by the last change made in the tool.|
|Gray text color|Indicates that the bitfield is not edited and the value is the after-reset value.|
|Black text|Indicates the bit-fields that the tool modifies.|
```
**Note:** When the Peripherals tool is active and register initialization components are used, the user can perform manual changes to some of the displayed values.
**Note:** This view contains registers for the selected tool. The view uses registers as internal parameters but it might not handle all the register writes needed in the code. The register writes are done inside the SDK functions that are called by the generated code. There might be additional registers accessed in the SDK code during the setup process, and such register writes are not known to the tool and are not displayed in the registers view.
## Log view
The **Log** view shows user-specific information about MCUXpresso Config Tools operations. The **Log** view can show up to 100 records across all tools in chronological order.
Each log entry consists of a timestamp, the name of the tool responsible for the entry, severity level, and the actual message. If no tool name is specified, the entry was triggered by shared functionality.
You can filter the content of the **Log** view using the combo boxes to display only specific tool and/or severity level information. Filters in different tools can be set independently.
Buffered log records are cleared using the clear button. It affects **Log** views across all tools.
```{eval-rst}
.. figure:: _images/mcuxlog.png
:scale: 60%
:align: center
**Log view**
```
## Config tools overview
The **Config Tools Overview** provides you with general information about your currently active configuration, hardware, and project. It also provides a quick overview of the used/active and unused/inactive tools, generated code, and functional groups. By default, the **Config Tools Overview** icon is on the left side of the toolbar.
**Config Tools Overview** opens automatically when you create and open a new configuration. You can disable this behavior in the **Preferences**.
**Config Tools Overview** contains several items.
### Table Config Tools Overview
```{table} Config Tools Overview
:name: config-tools-overview
|Item|Description|
|----|-----------|
|**Configuration – General Info**|Displays the name of and the path to the MEX file of the current configuration. Click the link to open the folder containing the MEX file. To import additional settings, click the **Import additional settings into current configuration** button.|
|**Configuration – HW Info**|Displays the processor, part number, core, and SDK-version information of the current configuration.|
|**Project**|Displays toolchain project information.|
|**Pins/Clocks/Peripherals/TEE/Device Configuration**|Displays basic information about the **Pins**, **Clocks**, **Peripherals**, **TEE, and** **Device Configuration** tools.|
```
**Note:** If you have disabled a tool and want to reopen it, click the tool icon in the upper right corner or select it from the Main Menu. The **Config Tools Overview** opens automatically.
To enable/disable the tools, click the toggle button. You can navigate to the tools by clicking their icons. The following information about the tools is also available:
### Table Config Tools Overview
```{table} Config Tools Overview
:name: config-tools-overview
|Item|Description|
|----|-----------|
|**Generated code**|Contains the list of source-code files. Click the links to open the files in the **Code Preview** view.|
|**Functional groups**|Contains the list of the currently active functional groups. To select the groups in the **Functional groups** tab in the toolbar, select the relevant links.|
```
- To open a tool-specific overview, select **Views > Overview** from the main menu.
```{eval-rst}
.. figure:: _images/mcuxoverview.png
:scale: 40%
:align: center
**Config Tools Overview**
```
**Note:** Unsupported tools are not displayed in the overview.
## Config tools snippets
The **Config tools snippets** view can be opened in the Config Tools perspective. The snippets view shows snippets collected from the Peripherals tool. The snippets can be categorized. The hierarchy is controlled by the tool. Copy to the clipboard can be done via the toolbar action or context menu.
**Note:** In the current version, the **Config tools snippets** view is supported for the Peripherals tool only.