# LinkServer Release Notes ## 26.9.130 ### New features - Added **Energy Measurement** for MCU-Link Pro (and on-board probes with power measurement circuitry): capture and analyze target current, voltage, power, and energy. Available as a command-line reporting mode (`measure report`) and also as an interactive graphical interface (`measure gui`/`gui measure`, or `measure server` for a browser). See the [Energy Measurement](EnergyMeasurement.md) documentation. - Added `probe identify` command to blink the status LED of MCU-Link probes in a distinctive pattern for visual identification (needs MCU-Link firmware V3.174 or newer). - Added `reset` command to reset the target device from the command line without starting a *GDB* session. - Upgraded MCU-Link version to 3.174. - Added initial support for FRDM-IMXRT1152 board and MIMXRT1152, MIMXRT1151 devices. - Added initial support for FRDM-MCXN947T board (FlexSPI flash loader not available for this target). - Added initial support for MIMXRT2660-EVK board and MIMXRT2663, MIMXRT2662, MIMXRT2661, MIMXRT2660 devices. - Added support for FRDM-IMXRT700 board. - Added support for KW43-LOC, MCXW70-LOC boards. - Added Cortex-M debug support for i.MX 937. - Added Cortex-M debug support for FRDM-IMX952 board. - Added support for MCXN526T, MCXN246 devices. - Added support for MCXW343, MCXW345 devices. - Added standalone entries (no board) for **Kinetis** devices: - **KW4x**: KW45Z41052xxxA - **KE1x**: MKE12Z512xxx9, MKE13Z512xxx9 - Added support for other **Kinetis** device families: - **K** (Kx): K10, K11, K12, K20, K21, K22, K24, K26, K27, K30, K40, K50, K51, K52, K53, K60, K63, K65, K70 - **KE**: KE04, KE14, KE16, KE18 - **KL**: KL02, KL03, KL13, KL14, KL15, KL16, KL17, KL24, KL25, KL26, KL27, KL33, KL34, KL36, KL43, KL46 - **KS**: KS20, KS22 - **KV**: KV10, KV30, KV31, KV42, KV44, KV46, KV56, KV58 - **KW**: KW21, KW22, KW31, KW34, KW35, KW36, KW37, KW38, KW39, KW41 - **QN**: QN9030 - Added support for CoreSight SoC-600. ### Improvements - Extended the `help` command with a `-a`/`--all` flag that prints the full help for every command and subcommand at once. - Reorganized the bundled device database into a family-based folder layout and migrated all definitions to schema 2.0.0, with boards and devices defined as separate, reusable fragments. Updated compatible devices information for all boards. - The `devices` command now lists a board and all of its compatible devices on a single line. A new **Other Compatible Devices** column shows the compatible devices. Standalone (board-less) entries are hidden for devices available through a board. Use `--all` to list every entry. - Simplified target selection: specifying only a board (for example `:FRDM-MCXA343`) now selects that board's default device, and appending `:` to a device name (for example `MCXA343:`) selects the matching board variant. - Added support for switching from JTAG to SWD via the dormant state. - It can be configured from the device JSON using the `/debug/swj-switching` property. - It can be configured from *redlinkserv* via the `probeconfig` command, using the `swj_switching` property. - Improved probe listing speed (noticeable on Linux with multiple probes connected). - Updated the multicore debug support for MCXE32x devices. - Enhanced the MCXL2xx preconnect script to avoid incorrect selection of the secondary core when launching debug on the primary core. - Added SWO trace support for KW43 and MCXW70 devices. - Flash drivers for KW43 and MCXW70 now disable glitch detection. ### Bug fixes - Fixed flash size detection for some MCXAxxx devices. - Resolved a FreeRTOS thread awareness defect that caused GDB debug sessions to fail for applications built with `configUSE_MINI_LIST_ITEM = 0`. - Fixed GDB stack unwinding failures after floating-point usage on Cortex-M cores, by adding the ARM Private Peripheral Bus (PPB) region, in the memory map reported by the GDB server. - Fixed probe discovery sometimes taking several seconds on Windows when an unrelated USB device connected to the host is in a low power state. ## 26.6.137 ### New features - Added Cortex-M debug support for FRDM-IMX95 board. - Added initial support for FRDM-KW43 and FRDM-MCXW70 boards. - Added initial support for FRDM-MCXE32B board and MCXE32B, MCXE327 devices. - Added flash loader for the external flash on FRDM-MCXA577 and FRDM-MCXA287 boards. - Device JSON files can now use schema version 2.0.0. - In the new version, devices and boards can be defined in separate files. - Boards now map to their supported device IDs. - LinkServer remains compatible with files using version 1.x.x. - Added MIMXRT1180 flash loader for HyperFlash on FlexSPI1. ### Improvements - Added info message when MCU-Link probes with SWD disabled are detected. - Fixed LinkServer hanging when the underlying redlinkserv exits abnormally. - Improved handling of sections placed in RAM and incorrectly marked as loadable in pure flash images. ### Bug fixes - Resolved flash programming issues with unaligned sizes. ## 26.5.59 ### New features - Added support for MCXN947T, MCXN946T, MCXN557T, MCXN556T, MCXN547T, MCXN546T, MCXN537T, MCXN536T, MCXN527T, MCXN247T, MCXN246T devices. - Added initial support for FRDM-MCXC162 board and MCXC162, MCXC161, MCXC151, SC6683 devices. - Added support for MCXA557 device. - Added Cortex-M debug support for i.MX943. ### Improvements - Updated the MCXE31x scripts to use subroutines from a shared common script. - Added support for using FlexSPI alias address ranges on MIMXRT1180 devices. - Enhanced support for flash size detection in the MCXL25x flash loader. - Improved MCU-Link probe detection following a firmware update. - The *redlinkserv* `LOAD` command now supports loading scripts relative to the LinkServer binaries directory (usage: `LOAD <"@LS_BIN_DIR@FILENAME">`). - Enhanced handling of GDET in flash driver and scripts for MCXA28x/4xx/5xx devices. ### Bug fixes - Fixed MIMXRT1180 Micron octal flash loader. ## 26.3.123 ### New features - Added Cortex-M debug support for i.MX 952. - Added Cortex-M debug support for i.MX 93W. - Added initial support for FRDM-MCXA287 board and MCXA286, MCXA287 devices. - Added initial support for FRDM-MCXA577 board and MCXA456, MCX457, MCXA536, MCX537, MCXA556, MCX566, MCXA567, MCX577 devices. - Added standalone entries (no board) for MIMXRT1185, MIMXRT118C devices. - Added standalone entries (no board) for MIMX9534, MIMX9536, MIMX9546, MIMX9546, MIMX9554, MIMX9556, MIMX9574, MIMX9576, MIMX9586, MIMX9594, MIMX95N4, MIMX95N6 devices. - Added support for MCXA183, MCXA184, MCXA353, MCXA354 devices. - Added support for MCXL142, MCXL143, MCXL144 devices. - *redlinkserv* is now shared between all LinkServer processes, resulting in performance improvements, especially for the `probes` command. - *redlinkserv* continues running for 10 seconds after LinkServer finishes, which speeds up the performance of consecutive operations. - Removed `--redlink-telnet-port` option. The default *redlinkserv* telnet port is now `23025` and can accept multiple concurrent connections. - Added a global configuration file for configuring default port ranges internally used by LinkServer. - `--config` option allows specifying a custom path for the configuration file, instead of using the default one. - [CLI, LinkFlash] Added command `flash erase-range` for erasing all flash sectors that overlap a given range. ### Improvements - Included IMX95-EVK board among the supported i.MX95 boards. - Enhanced the MCXE31x connect and reset scripts to support password-based debug authorization mode. - Enhanced target connection support for custom debug settings (AP indexes, JTAG TAP IR length, unlock keys). - Various improvements to LinkServer installer on Windows (modern look, dark mode support, 64-bit, enforce x64 architecture check, allow installation without creating shortcuts). - Upgraded MCU-Link version to 3.172 and LPCScrypt version to 2.1.4_101 due to Windows installer updates. ### Bug fixes - Fixed JTAG connection issues for i.MX 95 B0 devices. - Fixed a potential deadlock when booting or hot-plugging probes in Linux. - Fixed port conflicts when multiple LinkServer processes are running in parallel. - Fixed potential issues with flash programming when mass erase before programming is enabled. ## 25.12.83 ### New features - Upgraded MCU-Link version to 3.167. - New Linux ARM64 host architecture support. - Upgraded LPCScrypt version to 2.1.4_98. - Added support for MCXN557S device. - Added support for MCXA173, MCXA174 devices, and FRDM-MCXA174 board. - Added preliminary support for Cortex-M55 and Cortex-M85 cores. - Added standalone entries (no board) for **Kinetis** devices from the following families: - **K32L2A41A**: K32L2A31xxxxA - **K32L2B11A**: K32L2B11xxxxA - **K32L2B21A**: K32L2B21xxxxA - **KW4x**: KW45B41Z52xxxA, KW45B41Z53xxxA, KW45B41Z82xxxA, KW45Z41053xxxA, KW45Z41082xxxA, KW45Z41083xxxA - **K0x**: MK02FN64xxx10, MK02FN128xxx10 - **K2x**: MK22FN128xxx10, MK22FN128xxx12, MK22FN256xxx12 - **KE1x**: MKE12Z128xxx7, MKE12Z256xxx7, MKE13Z128xxx7, MKE13Z256xxx7, MKE14Z128xxx7, MKE14Z256xxx7, MKE14Z32xxx4, MKE14Z64xxx4, MKE15Z32xxx4, MKE15Z64xxx4 - **KM3x**: MKM14Z64Axxx5, MKM14Z128Axxx5, MKM33Z64Axxx5, MKM33Z128Axxx5 - Added RT1180 flash drivers for Micron Octal flash. - [CLI, LinkFlash] Added support for selecting which flash memories to erase (if there are multiple). - [CLI] Added `gdbserver --no-rtos` option for disabling RTOS thread awareness. ### Improvements - New MCU-LINK_installer build for macOS with native Apple silicon support. - New LPCScrypt build for macOS with native Apple silicon support. - General performance improvements for LinkServer. - Probes configured with the debug function disabled are no longer listed. - Added *Capabilities* column to `probes` output. - Added `probes --capab` option for filtering probes with specific capabilities. - Replaced `flash regions` command with `device info`. The new command no longer requires a connected probe. - Replaced `config` command with `device export`. Replaced the `--output` option with a mandatory positional argument. ### Bug fixes - Fixed hang when WINUSB-based probes fail to communicate. - Fixed intermittent hang when using the HID-based probes with latest macOS version. - Fixed port allocation issue when IPv6 is disabled. - Fixed handling of Ctrl-C and `--pause` in runner. - Fixed potential heap corruption during flash programming. - Fixed placing XMCD data inside the boot header section of RT1170/RT1160 targets. - Fixed SYSRESET being ignored from non-secure state. ## 25.9.134 ### New features - Upgraded MCU-Link version to 3.165. - Added initial support for MCXA185, MCXA186, MCXA265, MCXA266 devices, and FRDM-MCXA266 board. - Added initial support for MCXA343, MCXA344 devices, and FRDM-MCXA344 board. - Added initial support for MCXA365, MCXA366 devices, and FRDM-MCXA366 board. - Added initial support for MIMXRT1186 device and FRDM-IMXRT1186 board. - Added support for MCXN247, MCXN526, MCXN527, MCXN536, MCXN537, MCXN556S devices. ### Improvements - Improved MCXE31x reset script for cases like post-download reset after flash erase. - Switched to using rapid blhost (rblhost) utility. ### Bug fixes - Updated the MCXE31x connect script to use part specific SRAM size for SRAM ECC initialization. - Resolved an issue with TCM1 memory access during Debug mode on MCXE31x devices. - Fixed `ConnectionResetError` after low-level `wireswdconnect` command. - Fixed desktop shortcut creation on Windows for non-admin users with space in their name. - Fixed probe booting with the latest macOS version. - Improved error message related to specifying devices on the command line. ## 25.7.33 ### New features - Added initial support for MCXL255, MCXL254, MCXL253 devices, and FRDM-MCXL255 board. ### Improvements ### Bug fixes - Updated RT1060 QSPI flash loader to work with updated FCB settings in SDK 25.09 for MIMXRT1060-EVKB boards. ## 25.6.131 ### New features - Upgraded MCU-Link version to 3.160. - Upgraded blhost version 3.0.0 (spsdk) - Added support for MCXW235, MCXW236 devices. - Added initial support for MCXA345, MCXA346 devices, and FRDM-MCXA346 board. - Added initial support for MCXA175, MCXA176, MCXA255, MCXA256, MCXA355, MCXA356 devices. ### Improvements - Updated RT1160/RT1170 support for rev C0 devices. - Added SWO trace support for MCXE31x devices. - Updated MCXE31x support to hide the secondary Cortex-M7 core (not present on these devices). - Added support to allow custom pre-attach initializations (needed for MCXE31x devices). - Added --exit-timeout option for runner to limit the time it waits for application termination. - Reduced installation size and remove reboot prompts on Windows. - Upgraded LinkServer launcher to use Python 3.13.3. - Upgraded libexpat version 2.7.1. - Discontinued support for legacy RedProbe and RedProbe+ probes. - Improved device verification based on CMSIS-DAP target information (if available). - Updated visual style for product icons. ### Bug fixes - Fixed a problem that can affect RT700 connections when multiple probes are connected to the PC. - Fixed a problem preventing LinkFlash to start when auto-saved configuration references missing files. - Fixed a problem related to an incorrect command sequence being displayed for LinkFlash Save operations. - Fixed a problem related to terminal settings handling in the runner when stdin is not connected to a terminal. ## 25.3.31 ### New features - Upgraded MCU-Link version to 3.156. - Added initial support for FRDM-MCXW23 and MCXW23-EVK. - Added initial support for MCXE247, MCXE246, MCXE245 devices, and FRDM-MCXE247 board. - Added initial support for MCXE31B, MCXE317, MCXE316, MCXE315 devices, and FRDM-MCXE31B board. - Added possibility to associate LinkServer with existing MCUXpresso IDE installations at install time. ### Improvements - Added new maintenance command for GUI management of integration with MCUXpresso IDEs. - Added standalone entries (no board) for **MCX** devices from the following families: - **MCXC14x/24x/44x**: MCXC141, MCXC142, MCXC143, MCXC144, MCXC242, MCXC243, MCXC244, MCXC443, MCXC444 - **MCXW7XX**: MCXW716AxxxA - Added standalone entries (no board) for **LPC** devices from the following families: - **LPC546XX**: LPC54605J256, LPC54605J512, LPC54606J256, LPC54606J512, LPC54607J256, LPC54607J512, LPC54616J256, LPC54616J512 - **LPC540XX**: LPC54S005, LPC54S016, LPC54005, LPC54016, LPC54018J2M, LPC54018J4M - **LPC550x/S0x**: LPC55S04, LPC5502, LPC5504, LPC5506 - **LPC551x/S1x**: LPC55S14, LPC5512, LPC5514, LPC5516 - **LPC552x/S2x**: LPC55S26, LPC5526, LPC5528 - **LPC553x/S3x**: LPC5534, LPC5536 - **LPC55S6x**: LPC55S66 - **LPC86x**: LPC864 - Added standalone entries (no board) for **i.MXRT** devices from the following families: - **MIMXRT500**: MIMXRT533S, MIMXRT555S - **MIMXRT600**: MIMXRT633S - **MIMXRT700**: MIMXRT735S - **MIMXRT1050**: MIMXRT1051B - **MIMXRT1060**: MIMXRT1061A, MIMXRT1061B, MIMXRT1064B, MIMXRT1165 - **MIMXRT1170**: MIMXRT1171, MIMXRT1172, MIMXRT1173, MIMXRT1175, MIMXRT117T, MIMXRT117H, MIMXRT117F, MIMXRT117C - **MIMXRT1180**: MIMXRT1181, MIMXRT1182, MIMXRT1187 - Added standalone entries (no board) for **i.MX** devices from the following families: - **MIMX93xx**: MIMX9301, MIMX9302, MIMX9311, MIMX9312, MIMX9321, MIMX9331, MIMX9332, MIMX9351 - **MIMX959x**: MIMX9596 - Added FlexSPI2 flash loaders for RT1180. - Improve USB probe listing performance on Windows. - LinkServer flash and run commands detect file type automatically for unknown file extensions. ### Bug fixes - Fixed LinkServer runner sending incorrect line ending when the user presses ENTER interactively in the console on Windows. - Fixed LinkServer runner `--pause` option requiring multiple key presses. - Fixed programming MCXA2xx/MCXA3xx parts, which reserve the final part of the flash range for Secure Installer functionality. - Fixed debug connection to KL28Z and LPC51U68 devices. - Fixed LinkServer inadvertently reusing the same (telnet) port in multiple concurrent instances. - Fixed handling of semihosting operations where the parameter block can start on unaligned target addresses. ## 24.12.21 ### New features - Upgraded MCU-Link version to 3.153. - Added initial support for KW47, MCXW72 devices, and KW47-EVK, KW47-LOC, MCX-W72-EVK, FRDM-MCXW72, MCX-W72-LOC boards. - Added Cortex-M debug support for i.MX 95 and i.MX 93. ### Improvements - Documented [LinkServer GDB server](GDBServer.md) monitor commands. - Documented [LinkServer integration with IDEs](IntegrationWithIDEs.md). - Added inline format description inside [binaries/Scripts/probetable.csv](binaries/Scripts/probetable.csv) file. - Added option for runner to wait for a specific marker before sending (non-interactive) input to the application. - Added interactive input capability to the runner. - Added LinkServer auto device selection and verification based on CMSIS-DAP target information (if available) - Added LinkFlash launcher and updated the installer to create LinkFlash shortcuts. - Added LinkFlash auto device selection and verification based on CMSIS-DAP target information (if available) - Added new maintenance commands category and subcommands for managing integration with MCUXpresso IDEs. - Updated override option to allow creating intermediary paths. - Added support for using shorter/simpler names as alternatives to ids for target device selection. - Replaced usage of .vbs scripts with PowerShell scripts due to VBScript deprecation in Windows. - Updated several LinkServer scripts (.scp) to reduce the wire speed temporarily while performing reset. - Improved locating preconnect, connect, and reset scripts relative to current directory. - Added standalone entries (no board) for MIMXRT1040 devices (MIMXRT1041, MIMXRT1042, MIMXRT1043, MIMXRT1046). ### Bug fixes - Fixed missing RAM regions for MIMXRT1160 and MIMXRT1170. - Updated the connect scripts and flash drivers for MIMXRT1180 to avoid flash driver initialization issues in some circumstances. - Updated MIMXRT1180 memory map (flash regions declared as Cortex-M33 regions) to allow debug of standalone Cortex-M7 examples in RAM. - Correctly identify reset context passed to reset scripts when multiple flash ranges are present (this was affecting secure flash images on RT700). - Fixed a problem seen in certain circumstances for list probes command (caused by some USB devices reported on Windows). - Fixed some problems related to obtaining dapinfo from probes. ## 24.9.75 ### New features - Upgraded MCU-Link version to 3.148. - Added initial support for MIMXRT700. - Add LinkServer flash programming utility for executing flash operations using the graphical user interface. - Refer to [LinkFlash](LinkFlash.md) for additional details regarding the GUI flash support. - Add LinkServer application runner for use in CD/CI testing environments. - LinkServer flash load and flash verify commands now accept multiple files as arguments. ### Bug fixes - Fixed a MCXN9xx FlexSPI flash driver problem (reproducible on some FRDM-MCXN947 boards). - Fixed RT1020, RT1160/RT1170/RT1180 flash drivers in SDP mode. ### Improvements - LinkServer binaries are now compiled as 64-bit applications on Windows. - Install x86 and x64 versions of Microsoft Visual C++ Redistributable on Windows. - Added MCXN9xx FlexSPI flash driver to examples. - Added disable GDET sequence to MCXN9xx and MCXN5xx preconnect scripts. - Added standalone entries (no board) for MCXN9xx, MCXN5xx, MCXN2xx, MCXA1xx devices. ## 1.6.133 ### New features - Added support for FRDM-MCXW71 board. ## 1.6.121 ### New features - Upgraded MCU-Link version to 3.146. - Added support for MCXC041, MCXC242, MCXC444 devices, and FRDM-MCXC041, FRDM-MCXC242, FRDM-MCXC444 boards. - Added support for MCXW71x devices and FRDM-MCXW7X board. - Added support for FRDM-RW612 board. - Added initial support for FreeRTOS v11 and newer FreeRTOSDebugConfig. ### Improvements - Increased the maximum number of supported probes in redlinkserv from 8 to 16. - Updated RW612 debug support for A2 silicon. - Updated LinkServer installer on Linux to keep multiple instances. ### Bug fixes - Fixed the message reported on list probes command when server error 0xAB occurs (Exceeded maximum number of connected probes). - Fixed problems related to evaluation of complex expressions in LinkServer scripts (.scp). - Fixed a problem related to soft reset for MIMXRT1170 and MIMXRT1160 when debugging Cortex-M4 applications in RAM. - Fixed a problem related to restart after flash load. ## 1.5.30 ### New features - Upgraded MCU-Link version to 3.140. - Added support for FRDM-MCXA156. - Added flash support for S19 and Intel Hex files. ### Improvements - Fixed execution via PATH on Linux and macOS. - Updated probes listing on Windows to show the MCU-Link probes opened by another LinkServer process. - Updated memory configuration for several devices (based on Cortex-M33) to include the secure RAM regions. - Automatic firmware update support for MCU-Link Mini probes. - Added an option for rltool to set the redlinkserv port. ## 1.4.85 ### New features - Upgraded MCU-Link version to 3.133. - Added support for FRDM-MCXN947. - Added support for MCXN2xx devices and FRDM-MCXN236 board. - Added support for automatic firmware update for MCU-Link probes. - Added support to show CMSIS-DAP probe information. - Added probe commands to run a low-level script, issue a timed reset. - Added support to dump the content of a flash region to a file. - Added ProbeReset and ProbeDAPInfo commands to redlinkserv. - Integration support for MCUXpresso IDE 11.9.x and later. The following artifacts have been moved from IDE within LinkServer installation: - CoreSight components configuration files: [binaries/coresight](binaries/coresight/). - LPC-Link2 power measurement circuits configuration files: [binaries/power](binaries/power/). - Default linker templates (.ldt) files: [Wizards/linker](Wizards/linker/). - Flash driver examples: [Examples/Flashdrivers](Examples/Flashdrivers/). ### Improvements - Updated the connect scripts for MIMXRT1180. - Flush the cache before reading memory for semihosting operations. ### Bug fixes - Fixed other problems related to flash blank command in GDB server and flash drivers (LPC55xx). - Fixed a semihosting file operation problem (wrong file position after SYS_FLEN system call). ## 1.3.15 ### New features - Upgraded MCU-Link version to 3.128. - Added support for KE1xZ512 devices and X-FRDM-KE17Z512. - Added support for MIMXRT1180-EVK board. - Added support for MCXA153 device and FRDM-MCXA153 board. - Added support for API versioning (MAJOR.MINOR), intended to be used for compatibility checks. ### Improvements - Log flash output to stdout. - Document the Flash drivers support. - Added --keep-alive option for gdbserver. ### Bug fixes - Correction of flash driver for eeprom flash locations in CTN73x/PN73xx/PN74xx. - Correction of RW61x connect script (ignore secure bit in entry address range check). - Fixed issues with `--script=` argument for redlinkserv. - Fixed issues with memory regions overlap between cores. - Fixed some problems related to the flash blank command. ## 1.2.45 ### New features - Upgraded LPCScrypt version to 2.1.3_83. - Upgraded MCU-Link version to 3.122. - Upgraded LinkServer LPC-Link2 firmware v5.460, which offers support for powering RT1xxx EVK boards through the USB debug connection. - New LinkServer build for Mac with native Apple silicon support. - Added support for MCXN9xx. - Added support for RW61x. - Added support for some missing (legacy) boards. ### Improvements - Removed the kits from the boards list. - Document the low-level functions and scripting support. - Erase each flash region only once. - Enable register caching on GDB $p packet. - Kinetis resurrect is missing for a few devices. ### Bug fixes - Flash tool not writing flash config. section from ELF. - Overflow problems in DAP_Transfer commands. - Problems related to semihosting operations. - Cannot boot LPC-Link1 when a LPC-Link2 probe configured for DFU booting is also present. ## 1.1.16 ### Improvements - Install VS2015 C++ Redistributable on Windows. ### Bug fixes - Secure flash regions are missing. ## 1.0.9 (First release)