.. Copyright 2026 NXP NXP Confidential and Proprietary. This software is owned or controlled by NXP and may only be used strictly in accordance with the applicable license terms. By expressly accepting such terms or by downloading, installing, activating and/or otherwise using the software, you are agreeing that you have read, and that you agree to comply with and are bound by, such license terms. If you do not agree to be bound by the applicable license terms, then you may not retain, install, activate or otherwise use the software. .. LinkServer Documentation master file. LinkServer Documentation ======================== `LinkServer `_ is a tool designed to launch and manage GDB servers for NXP debug probes. It offers both graphical and command-line interfaces for programming target flash memory, along with an integrated test runner for automated workflows. It can be used within NXP MCUXpresso for Visual Studio Code, with custom GNU-based debug setups, or in headless environments for continuous integration and testing. LinkServer can be used with CMSIS-DAP probes such as `MCU-Link `_, `LPC-Link2 `_, LPC11U35-based and OpenSDA-based standalone or on-board debug probes from NXP. **System Requirements:** * **Windows** (x86-64): Windows 10 and 11 * **Linux** (x86-64 or ARM64): Ubuntu 20.04.2 LTS / 22.04 LTS / 26.04 LTS * **Mac** (Intel or M-series): macOS 13.x Ventura / 14.x Sonoma / 15.x Sequoia / 26.x Tahoe **License:** `NXP software license agreement `_ Table of Contents ================= .. toctree:: :maxdepth: 1 :caption: Release Notes ReleaseNotes .. toctree:: :maxdepth: 1 :caption: LinkServer Readme .. toctree:: :maxdepth: 1 :caption: LinkFlash LinkFlash .. toctree:: :maxdepth: 1 :caption: CI/CD Runner Runner .. toctree:: :maxdepth: 1 :caption: Advanced Information IntegrationWithIDEs GDBServer FlashDrivers LowLevelFunctions ScriptingSupport MiscellaneousConfigurations Useful Links ============ * `MCUXpresso Installer `_ * `MCUXpresso for Visual Studio Code `_ * `MCUXpresso IDE `_ * `MCU-Link debug probe `_ * `MCU-Link Pro debug probe `_ * `MCU-Link MR debug probe `_