# Working with Pure CMake Projects ## Pure CMake Projects SDKs built on the *[MCUXpresso SDK Builder](https://mcuxpresso.nxp.com/en/welcome)* support downloading standalone examples, as opposed to the full SDK archive. These standalone projects do not require an SDK, instead relying only on CMake and the included files. ## Downloading a pure CMake project After building an MCUXpresso SDK, open the download section and select the *Download Standalone Example Project* option. ![Download Standalone Example Project](./pictures/nxp-download-standalone-project.png) Select the desired example project and click on *Download Example*. ## Importing a pure CMake project The project archive can be imported by opening the *Import Project* menu in the **Quickstart Panel**. The *Import path* should be the downloaded archive. ![Import Pure CMake Project](./pictures/nxp-import-pure-cmake-project.png) The project can be built just like any other project, however debugging it will open a wizard to ask for more information since there is no associated repository. ## Associating a repository Associating a repository to a pure CMake project is optionally, but it can be done by entering the context menu of the project and selecting the *Associate Repository* option under the *Configure* tab of the menu. Two quick picks will be, then, shown to select the repository to associate to and the target device. ![NXP Associate Repository](./pictures/nxp-associate-sdk.png) ## Building and debugging the project For building and debugging the project, the standard steps described in {ref}`Build Project ` section and [debug](./Debug.md) documentation sections should be followed.