# Debug Views ## Run Control ### Debug Toolbar Once a debug session starts, the **Debug toolbar** will appear on the top of the window. ![Debug Toolbar](pictures/nxp-debug-toolbar.png) MCUXpresso for VS Code extension contributes custom actions like **Reset device** and **Enable instruction stepping mode** / **Disable instruction stepping mode**, alongside the [Standard debug actions](https://code.visualstudio.com/docs/editor/debugging#_debug-actions) provided by Visual Studio Code. **Reset device** can be used to issue the commands required for a target reset. `preResetCommands` and `postResetCommands` can be used in the launch configuration to execute GDB commands before and after the reset. After the target is reset, execution is resumed until it reaches the symbol specified by `stopAtSymbol` (`main` by default). *Restart vs Reset*: `Restart` simply terminates the current debug session and starts debugging again using the same launch configuration. `Reset` is usually preferred because it is faster and more meaningful. **Enable instruction stepping mode** / **Disable instruction stepping mode** control the enablement of instruction stepping mode during a debug session. Once enabled, the **Disassembly** view is automatically started and stepping is performed at instruction level, depending on the step operation that is executed. Enablement of instruction stepping is also taken into account when stepping while having a source editor active. Once the debug session is terminated, instruction stepping mode is automatically disabled for subsequent debug sessions. ![Source file context menu](pictures/nxp-instruction-stepping-mode.png) ### Context menu Right clicking inside a source file during debugging reveals two more run control actions: - **Run to Cursor**: Place a temporary breakpoint on the cursor's location and resume execution. - **Jump to Cursor**: Move the instruction pointer to the cursor's location. ![Source file context menu](pictures/nxp-context-menu-run-control.png) (variables)= ## Variables **Variables** view is automatically populated when a debug session starts. It displays all the available variables in 4 major groups: Local, Global, Static and Registers. ![Variables View](./pictures/nxp-variables-view.png) All these variables can be accessed by the debug chain (read and potentially written) while the debug session is paused. The value of the variable displayed corresponds to the value in memory. Optional, the values can also be displayed as hex: ![Values as hex](./pictures/nxp-variables-hex.png) The values of the static variables will be available when the debug session will be paused in the corresponding source file: ![Static Variables](./pictures/nxp-variables-static.png) Tooltip of each variable shows various details, like its type, its location in memory or the hex/dec/oct/bin encondings. ![Tooltip Variables](./pictures/nxp-variables-tooltip.png) Right-click menu on variables shows a list of actions. The variable value can be changed, the variable can be copied as value or expression, the location of the variable can be copied and also, a Memory Inspector editor can be started by using the location of the variable. Moreover, it can be used to set data breakpoints (watchpoints): ![Variables Menu](./pictures/nxp-variables-menu.png) Any variable can be added to **Watch** view and any global and static variables can be added to **Live Watch** view. The **Variables** view toolbar also exposes a **Show in Memory Inspector** action (circuit board icon) that opens the {ref}`Memory Inspector ` panel directly, without needing to go through the command palette. The panel is opened with no pre-filled address, so you can then type the address or expression you want to inspect. ![Memory View Variables Toolbar](./pictures/nxp-memory-view-toolbar.png) ## Breakpoints When the debugger starts, it automatically sets an initial breakpoint on the first statement in `main()` if the default launch configuration is used. ![Main Breakpoint](./pictures/nxp-main-breakpoint.png) If desired, you can change where this initial breakpoint is set by changing `stopAtSymbol` in the launch configuration. To disable the initial breakpoint, remove `stopAtSymbol` in the launch configuration. When viewing the source during a debug session, you can toggle breakpoints by simply clicking in the leftmost side of the source view. You can do this when the target is paused or running. ![Setting Breakpoints](./pictures/nxp-setting-breakpoint.png) Breakpoints are displayed in the **Breakpoints** view. You can use this view to add, delete, modify or disable the breakpoints. MCUXpresso for VS Code supports two types of breakpoints: - Regular - this is the default breakpoint type, meaning that the actual type (software, hardware) is decided by the debug adapter and the debug server, depending on the executing context. - Hardware - this is usually used while debugging code in flash but other use cases might also require this type of breakpoints. By default, "Regular" breakpoints are installed on target but this is configurable through the command palette (Ctrl-Shift-P). Type "Select default breakpoint type" and you'll be able to choose between the two types available. The default type is also configurable directly through the **Breakpoints** view. ![Select Default Breakpoint Type](./pictures/nxp-default-breakpoint-type.png) The **Breakpoints** view allows per-breakpoint configuration and each breakpoint can have a different type. In order to change the type, right-click a breakpoint and then select Edit Mode. ![Select Breakpoint Type](./pictures/nxp-edit-mode-breakpoint.png) A quick-pick will ask you for the desired breakpoint type. ![Select Breakpoint Type Quick-Pick](./pictures/nxp-select-break-type.png) For easy identification, each breakpoint entry from the **Breakpoints** view is decorated with the actual breakpoint type configured. By default, VS Code does not require a specific breakpoint type, thus the entries might not be decorated with any breakpoint type. However, these are assimilated with the default type configured using the command described above. For more details follow [Breakpoints documentation](https://code.visualstudio.com/docs/editor/debugging#_breakpoints) provided by Visual Studio Code. ![Breakpoints view](./pictures/nxp-breakpoints-view.png) When a project is removed from the workspace, or permanently deleted from the disk, the source breakpoints associated to the project, and set during a previous debug session will be automatically removed from the **Breakpoints** view. ## Data Breakpoints (Watchpoints) The application can be stopped in debug by using code breakpoints but also by using data breakpoints, also known as watchpoints. Watchpoints can be useful to debug the application when a variable is accessed (for example, read or written) or when a generic memory area is accessed (for example, read or written). One way to install a watchpoint is to right-click a variable inside the **Variables** view, then select one of the access type needed. An item associated to the watchpoint will also appear inside the **Breakpoints** view. ![Watchpoints for Variables](./pictures/nxp-watchpoint-for-variables.png) Watchpoints can also be installed by using raw/absolute addresses. This is useful when there is no variable associated to a given address and you still want to suspend application when that specific address is accessed (for example, debugging a stack overflow). To achieve this, use the dedicated action from the **Breakpoints** view. ![Watchpoints for Addresses](./pictures/nxp-watchpoint-for-addresses.png) You will be asked for the address range and for the type of the access (read, write, readWrite). Once all information is provided, the watchpoint will be listed in the **Breakpoints** view ![Watchpoints for Addresses](./pictures/nxp-breakpoints-view-with-watchpoint-for-addresses.png) ## Watch Variables and expressions can also be evaluated and watched in the Run and Debug perspective, in the **Watch** view. Expressions added inside the **Watch** view, are evaluated once the target is suspended in a breakpoint or watchpoint, or the Pause button from the Debug toolbar is pressed. The **Watch** view is visible in the Run and Debug perspective. The following screenshot illustrates the available toolbar buttons: 1. **Add Expression** button that allows adding a valid C/GDB expression. It can contain simple/plain variable names or complex C/GDB expressions (for example: castint to specific types, dereferencing pointers, accessing structure data members, and much more). 2. **Toggle between hex format and natural format**, used to display the results of the evaluations. The "natural" format is dictated by GDB. 3. **Remove All Expressions** from the view. 4. **Collapse All** child nodes expanded inside the view. ![Toolbar buttons inside the Watch view](./pictures/nxp-debug-watch-toolbar.png) ![Complex expressions inside the Watch view](./pictures/nxp-debug-watch-complex-expressions.png) New expressions can be also added by using the **Variables** view. Once right-clicking a variable inside the view, the "Add to Watch" context menu is displayed and can be used to add the variable to watched expressions. ![Add to Watch context menu inside Variables view](./pictures/nxp-debug-variables-add-watch.png) > **Note:** Expressions referencing local variables can only be evaluated when target is suspended inside the scope where the referenced local variables are available. Expressions that cannot be evaluated in a specific context will lead to error messages being displayed, as shown in the screenshot below. ![Expression not evaluated inside the Watch view](./pictures/nxp-debug-watch-evaluation-error.png) ## Live Watch MCUXpresso for VS Code extension also offers a **Live Watch** view that can be used for monitoring the values of specific global or static variables, without suspending the target. Given that it comes with an overhead during an active debug session, **Live Watch** functionality is disabled by default. When disabled, the view indicates this, as shown in the screenshot below. ![Live Watch disabled hint](./pictures/nxp-live-watch-hint-enable.png) In order to enable live monitoring for variables, you must first enable this feature. Open the `launch.json` file and then add the `liveWatch` node with the `enabled` attribute. ![Live Watch enabled via launch.json](./pictures/nxp-live-watch-launch-enable.png) Currently, **Live Watch** works only when dealing with an active debug session linked to a SEGGER J-Link debug probe, LinkServer and PEmicro being unsupported at this point. In case the feature is explicitly enabled on unsupported probes, a warning notification will be shown in VS Code and also the view will make it clear that it is not supported for the currently used debug probe. ![Live Watch unsupported warning notification](./pictures/nxp-live-watch-unsupported-linkserver-notification.png) In order to add variables inside the **Live Watch** view, there are several options: 1. Right-click a global variable inside the **Variables** view and use the dedicated context menu action. ![Add variable to Live Watch using the Variables view](./pictures/nxp-live-watch-add-from-variables.png) 2. Use the "+" button available in the view's toolbar and type the name of a global or a static variable. 3. Use the command palette (Ctrl-Shift-P), type "Add Expression to **Live Watch**" and then type the name of a global or a static variable. Once added, items from the view can be edited in place. In order to remove a variable, or reorder the items from the view, use the dynamic toolbar that is activated when hovering items inside the view. ![Remove and reorder variables inside Live Watch](./pictures/nxp-live-watch-organize-items.png) Once the debug session is resumed, the variables added inside the view are continuously evaluated and the values updated inside the view. Sampling rate is configured through the `launch.json` file by changing the value of `samplesPerSecond` attribute. Moreover, the refresh rate of the view is configured through the settings page. ![Refresh rate configured in settings page](./pictures/nxp-live-watch-settings.png) Note that the usefulness of "live" variables reduces as the number of variables monitored increases, and ultimately there is a limit as to how many variables can be updated at the selected frequency. ## RTOS Awareness RTOS thread-aware debugging is available in the **Call Stack** view once the scheduler has started. Thus, it does not appear straight after loading the application when the default breakpoint on `main()` is reached. ![Thread-aware Call Stack](pictures/nxp-rtos-thread-awareness.png) Thread-aware debugging is a feature specific to each debug solution (GDB server), thus there are small differences with regards to information presented in the **Call Stack**. Furthermore, **Segger** RTOS awareness needs to be manually enabled as described in the {ref}`Enabling section ` below. Debug works in stop mode. In other words, if the execution of a user task is halted either through a user action (halt) or a debug event (breakpoint, watchpoint, fault, and so on), the stopped thread is current and no application thread executes in the background. The register context for any thread is available in the {ref}`**Variables** ` view. For suspended or blocked threads, the registers that RTOS saves in memory before swapping out the thread will not change, regardless of which thread stack level is being examined within the **Call Stack** view. (enabling-rtos-awareness)= ### Enabling RTOS Awareness No configuration is necessary for **LinkServer** and **PEmicro**. For **Segger**, RTOS awareness must be manually enabled using the `gdbServerConfigs/segger/rtos` property in the debug configuration. The value must be set to the Segger RTOS plugin corresponding to the RTOS being used in the project. Auto-complete is available for known plugins provided by Segger. Example: ```json { "configurations": [ { ... "gdbServerConfigs": { ... "segger": { ... "rtos": "GDBServer/RTOSPlugin_FreeRTOS" ``` ### FreeRTOS Stack Unwinding Considerations FreeRTOS tasks should never return. To catch such errors, FreeRTOS sets the `LR` register of newly created tasks to `configTASK_RETURN_ADDRESS` macro, which, by default, is defined as `prvTaskExitError`. If a task ever returns, it jumps to the first instruction of `prvTaskExitError` instead of jumping to a random address. However, this behavior can cause issues when GDB unwinds the stack. Because `LR` is set to the first instruction of `prvTaskExitError`, GDB assumes that the previous `PC` is one instruction before, which belongs to a different function. After that, GDB may either stop or continue to unwind the stack erroneously depending on the particular function. Therefore, you may see bogus functions and addresses at the base of the stack for each task. Bad stack unwinding may cause memory reads from invalid addresses, which break the debug connection on some MCUs. These errors affect the ability to debug the application even in normal working conditions (that is, outside the case when a FreeRTOS task inadvertently returns). You can easily avoid the invalid memory reads by adding `#define configTASK_RETURN_ADDRESS 0` in the `FreeRTOSConfig.h` file. However, this change disables the ability to catch inadvertent task returns offered by `prvTaskExitError()`. A more advanced solution, which still maintains the advantage of being able to catch such programming errors, is to use a custom function designed to allow GDB to unwind the stack correctly by adding the following lines: In `FreeRTOSConfig.h`: ```c extern void taskReturnCatcher(); #define configTASK_RETURN_ADDRESS (taskReturnCatcher + 2) ``` In your main source file: ```c #include "portmacro.h" __attribute__((naked)) void taskReturnCatcher() { __asm volatile ("nop"); taskDISABLE_INTERRUPTS(); while(1); } ``` > **Note:** For west-based MCUXpresso SDK 24.12 or newer, the `FreeRTOSConfig.h` header file is not included in the imported project. Instead, create a `FreeRTOSConfig_frag.h` header file in the project's folder and add to it the definitions mentioned above. For this file to be included in the build process, append the following line to `prj.conf`: `CONFIG_FREERTOS_USE_CUSTOM_CONFIG_FRAGMENT=y`. If `prj.conf` does not exist, create it in the project's folder. ## Disassembly The **Disassembly** view allows the code of an application to be viewed at the assembly level (as generated by the compiler). The view can be enabled (if required) via the context menu in the editor. ![Memory View](./pictures/mcx-disassembly-menu.png) This has two functions, in that it both spawns the view and switches stepping mode from source level to assembly level. Assembly level stepping is typically used in conjunction with the **Variables** view to examine the detailed behavior of short pieces of code. Closing the **Disassembly** view will switch back to source stepping mode. The **Disassembly** view can also be open from Visual Studio Code's Command Palette by executing 'Open Disassembly View'. (memory-view-and-editor)= ## Memory View and Editor MCUXpresso for VS Code extension integrates Memory Inspector, a memory viewer extension provided by Eclipse CDT Cloud. ![Memory View](./pictures/nxp-memory-view.png) Once a debug session is started, this view can be opened in several ways: - Type "Memory Inspector" in the command palette (Ctrl-Shift-P) and select **Memory: Show Memory Inspector**. - Click the **Show in Memory Inspector** button (circuit board icon) in the **Variables** view toolbar. This opens an empty Memory Inspector panel where you can manually enter the address or expression you want to examine. - Right-click an entry in the **Call Stack** view and select **Show in Memory Inspector**. The Memory Inspector panel opens pre-populated with the **Stack Pointer (SP)** address of the selected frame, which is useful for inspecting the memory layout of that frame's stack. ![Memory View Call Stack](./pictures/nxp-memory-view-callstack.png) > **Note:** Due to a Visual Studio Code limitation, you must first left-click the call stack frame to select it, and only then right-click it to open the context menu. If you right-click on a frame that is not the currently selected one, the Stack Pointer cannot always be resolved correctly. The **Show in Memory Inspector** actions require the [Eclipse CDT Memory Inspector](https://marketplace.visualstudio.com/items?itemName=eclipse-cdt.memory-inspector) extension to be installed. If the extension is not installed when you trigger the action, MCUXpresso for VS Code will prompt you to install it. If the extension is installed while a debug session is already running, that session must be restarted before the Memory Inspector can attach to the target; a notification with a **Restart Debug Session** button is offered for this purpose. ![Memory View Restart Install](./pictures/nxp-memory-view-restart-install.png) Check the _Advanced Display Options_ to customize the display format for the memory content. ![Memory View Settings](./pictures/nxp-memory-view-settings.png) For more details about how to use this view, please visit the official [Memory Inspector documentation page](https://github.com/eclipse-cdt-cloud/vscode-memory-inspector/blob/main/README.md). ## Baremetal Heap and Stack Usage Offers a utility for Stack and Heap status allocation at runtime for baremetal applications. Go to the [**Heap and Stack**](Heap-and-Stack) section for more details. ![Heap and Stack](./pictures/nxp-debug-heap-stack.png) ## Analysis In this version, **Analysis** view has the capability to load an existing [Energy Measurement](https://www.nxp.com/webapp/Download?colCode=MCUXPRESSO-EM) archive file (which was generated by the [MCUXpresso IDE](https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-integrated-development-environment-ide:MCUXpresso-IDE)) and to display the minimum, maximum and average values for the measured samples. ![Analysis](./pictures/nxp-analysis.png) Additionally, this view provides the SWO clock configuration utility as a setup prerequisites for working with [SWO ITM](SWO).