# Command line for MCUXpresso Installer
The MCUXpresso Installer tool offers command-line support for installing available tools or checking the status of installed ones. The MCUXpressoInstallerCLI executable is included alongside the GUI executable on all operating systems.
## Help command
* ``-h, --help`` - Display help for commands.
## Check updates command
* ``--check-updates`` - Check if MCUXpresso Installer has updates.
## Version command
* ``-v, --version`` - Display the application version.
## Install command
* ``install | i`` - Used to install packages and components from MCUXpresso Installer.
Options:
* ``-h, --help`` - Display help for install command. Provides details about options and the choices for arguments.

* ``-a, --all`` - install all packages available.
* ``-p, --packages `` - install one or more packages.
* ``-c, --components `` - install one or more components.
* ``-d, --dump [file]`` - export the installation log as JSON format. The user can provide the name of a new or existing JSON file. If no file is provided, a reports directory is created in a default location (the MCUXpresso Installer installation path) and a new file is created there. This file can be used in automation systems to identify components installation status. In the file, there are two details provided.
* envUpdate - marked as true when the MCUXpresso Installer added the component to the PATH of the user.
* exitCode - represents the installation status, 0 for success and any integer other than zero to indicate failure.
* ``--undo`` - undo the latest components installation.


## List command
* ``list | l`` - Used to give details about packages and components.
Options:
* ``-h, --help`` - display help for list command. Provides details about options and the choices for arguments.
* ``-a, --all`` - list all packages and the status of components.
* ``-p, --packages `` - this option has the possibility to see updates only for some packages.
* ``-c, --components `` - this option has the possibility to see updates only for some components.
* ``-d, --data`` - list the data from yaml files, which contains the relation between packages and components.

* ``-e, --export [path]`` - export the version report as JSON format. The user can provide the name of a new or existing JSON file. If no file is provided, a reports directory is created in a default location (the MCUXpresso Installer installation path) and a new file is created there. This file can be used in automation systems to identify packages and components status. In the file, there are multiple details provided:
* name: the name of the components
* level:
* "info" (no action needed)
* "warn" (update available)
* "error" (component not installed or it does not meet the required minimum version)
* installedVersion: the highest version found
* versionToBeInstalled: the version that can be installed using MCUXpresso Installer
```
{
"MCUXpresso SDK Developer": [
{
"name": "CMake",
"level": "error",
"installedVersion": "3.28.1",
"versionToBeInstalled": "3.30.0"
},
{
"name": "Ninja",
"level": "error",
"installedVersion": "",
"versionToBeInstalled": "1.12.1"
},
{
"name": "Git",
"level": "info",
"installedVersion": "2.39.0",
"versionToBeInstalled": "2.39.0"
},
{
"name": "Arm GNU Toolchain Standalone add-ons",
"level": "warn",
"installedVersion": "13.2.1",
"versionToBeInstalled": "13.2.4"
},
...
]
}
```
* ``-u, --updates`` - this option can be added to the command to show only the components that need updates.

**Note**: The list command uses multiple colors to highlight the status of components:
* default terminal color - the component is up to date
* yellow - an update is available
* gray
* the component is not installed
* the component is installed, but it does not meet the required minimum version
**Note**: Options that use package names as arguments support multiple package name formats.
* Full name "Arm GNU Toolchain" - Use double quotes when the package name contains spaces.
* Replace spaces with special characters or remove them to avoid using quotes - ArmGNUToolchain, Arm-GNU-Toolchain.
* The names of the packages are case insensitive: arm-gnu-toolchain.
* A package name can match multiple packages: "toolchain" can be used for "Arm GNU Toolchain" and "Standalone Toolchain Add-ons" at the same time.