# MCUXpresso Installer troubleshooting The **MCUXpresso Installer troubleshooting** guide is designed to help users quickly identify and resolve common issues encountered during the installation of development software tools dependencies. ## Table of Contents - {ref}`Python Virtual Environment ` - {ref}`Wget Utility ` - {ref}`Windows Developer Mode ` (python-virtual-environment)= ## Python Virtual Environment Issues can be encountered during the creation, updating, activation, or usage of the Python virtual environment. ### Common causes - Corrupted Python installation - Corrupted virtual environment - The existing virtual environment is tied to a missing Python installation ### Recommended solutions #### 1. If the virtual environment does not exist - Make sure that the correct version of **Python** is installed and functional under `%USERPROFILE% (or $HOME on Unix systems)/.mcuxpressotools/python-`. - Retry the creation of the virtual environment using the **MCUXpresso Installer**: - Open **MCUXpresso Installer**. - Perform a **check for newer versions of components**. - Install the **Python environment** for the desired package. #### 2. If the virtual environment exists - Remove the existing virtual environment from `%USERPROFILE%(or $HOME on Unix systems)/.mcuxpressotools/.venv`. - Retry the creation of the virtual environment using the **MCUXpresso Installer**. - Open **MCUXpresso Installer**. - Perform a **check for newer versions of components**. - Install the **Python environment** for the desired package. (wget-utility)= ## Wget utility Issues regarding the installation of **Wget** can occur on systems where network connectivity is restricted or proxy configurations are modified. ### Common causes - Incomplete or misconfigured network settings - Proxy server restrictions - Firewall blocking download connections - Invalid or outdated SSL/TLS certificates ### Recommended solution #### Manual wget download and configuration - Download Wget from an official mirror site - Add **Wget** to the **PATH** environment variable - Verify the installation by running `wget --version` in a new instance of the command prompt or terminal - To ensure that the new configuration takes effect, you have to restart the **MCUXpresso Installer** application (windows-developer-mode)= ## Windows Developer Mode Some development tools require Windows Developer Mode to be enabled for proper functionality, particularly for debugging and development features. ### Recommended solutions #### 1. Enable Developer Mode through Settings **Steps:** - Open **Settings** (Windows key + I) - Navigate to **System → For developers** (Windows 11) or **Update & Security → For developers** (Windows 10) - Select **Developer mode** - Click **Yes** when prompted to confirm the change - Restart your computer if prompted #### 2. Enable Developer Mode through Registry (if the Settings method fails) **Steps:** - Press **Windows key + R** and type `regedit` - Navigate to `HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\AppModelUnlock` - Create a **DWORD (32-bit) Value** named `AllowDevelopmentWithoutDevLicense` - Set the value to **1** - Restart your computer #### 3. Verify that Developer Mode is enabled **Steps:** - Open **Command Prompt** as administrator - Run the command: `reg query "HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\AppModelUnlock" /v AllowDevelopmentWithoutDevLicense` - Verify that the value is set to **0x1**