# Linked Projects Various software repositories offer mechanisms to generate one or multiple binary images to be integrated in more complex applications: multicore, TrustZone (with secure and none secure applications), libraries to be included in other projects, etc. This is the case when multiple projects contribute to the same target application. MCUXpresso for VS Code aims to help the user to handle such multiple project cases with full support for create/import projects, build full binary image, flash and debug. ## MCUXpresso SDK For MCUXpresso SDK, the MCUXpresso for VS Code extension detects the link required between various projects. One case is the multicore and TrustZone features exercised in a single application (example for LPC55S69/MCXN947): /multicore_examples/rpmsg_lite_pingpong_tzm, where three projects are linked: - cm33_core1 - project to generate the image for the secondary cm33 core of the LPC55S59/MCXN947 device - cm33_core0/ns - project to generate image for the non-secure part of the primary cm33 core of LPC55S69/MCXN947 - cm33_core0/s - project to generate image for the secure part of the primary cm33 core of LPC55S69/MCXN947 cm33_core0/ns is linked to cm33_core0/s because: - it also needs to build and flash secure image when building and debugging its own image. cm33_core0/s is linked to cm33_core0/ns ### TrustZone projects For more details on TrustZone projects using MCUXpresso SDK, see the [TrustZone Examples on LPC55S6x and MCUXpresso SDK 2.x](./TrustZone-Examples-on-LPC55S6x-and-MCUXpresso-SDK-2.x.md) or [TrustZone Examples on MCXN947 and MCUXpresso SDK 24.12](./TrustZone-Examples-on-MCXN947-and-MCUXpresso-SDK-24.12.md) reference guides.