MCUXpresso Task Definition

An MCUXpresso task, or a list of tasks, must respect a JSON schema defined by the MCUXpresso for VS Code extension. Files that respect the following pattern mcuxpresso-tasks*.json are automatically validated against the schema, when opened and edited within VS Code. Also, all tasks added in tasks.json that are MCUXpresso-specific (i.e. "type": "MCUXpresso") are also validated against the same schema.

There are multiple actions that can be performed using the MCUXpresso task system, and each of the actions requires a specific set of command options to be defined. The command options are defined within the commandOptions property of the task object.

MCUXpresso Task

Each task needs at least the "type", "version", "label", and "commandOptions" properties. The "runOptions" property is optional but it allows controlling the execution details of the task.

The sections below list the available commands and their required options.

High-level view of the basic properties

Property

Type

Required

Description

type

“MCUXpresso”

✓

MCUXpresso task type.

version

string

✓

MCUXpresso task version.

label

string

✓

The task label. This will be displayed in the Terminal view inside VS Code.

description

string

Optional description of the MCUXpresso task’s purpose and functionality.

id

string

Optional ID that can be assigned and help to uniquely identify the task within a sequence of tasks.

commandOptions

object (combined)

✓

See specific command details below

runOptions

object

Options that help controlling various aspects of the task execution.

    awaitPreviousTasksCompletion

boolean

Whether to wait for all the previous async tasks to complete before starting current task. By default, previous tasks are not awaited for completion.

    awaitTaskCompletion

boolean

Whether to wait for the task to complete before starting the next task. By default, task is awaited for completion.

    executionDelay

number

Delay execution of current task with the given number of seconds. By default, no delay is applied.

    executionTimeout

number

Timeout (in seconds) for current task execution. Task will be terminated once timeout occurs. A non-negative and non-zero value is valid. By default, no timeout is used.

    retryCount

number

If task fails, retry for the specified number of times. Retrying might help in certain setups, for example when retrieving data over an unreliable network connection. By default, no retries are performed.

    skip

boolean

Whether to skip the task. By default, task is executed.

    taskOutputFile

string

Path to a file that will contain the task’s output. By default, a temporary file is automatically created.

Available commands

The commandOptions property defines the specific command to execute and its parameters.

Base Command Property

Property

Type

Required

Description

command

“installDependencies” | “installRemoteRepo” | “installRemoteStandalonePackage” | “installLocalRepo” | “installLocalArchive” | “installAchProduct” | “uninstallRepo” | “importExampleFromRepo” | “importProject” | “createProject” | “removeProject” | “buildProject” | “cleanProject” | “rebuildProject” | “eraseFlash” | “programFlash” | “runDebugProject” | “westBuild”

✓

The MCUXpresso command to execute.

Description of individual commands

The section below provides details about each of the command type supported by the MCUXpresso for VS Code extension.

Command: "installDependencies"

Properties supported by the “installDependencies” command:

Property

Type

Required

Description

    command

“installDependencies”

✓

ID of the command.

    dependencyType

“sdkDeveloper” | “zephyrDeveloper” | “matterDeveloper” | “debugSupport”

✓

Types of dependencies valid for “installDependencies” task.

Command: "installRemoteRepo"

Properties supported by the “installRemoteRepo” command:

Property

Type

Required

Description

    command

“installRemoteRepo”

✓

ID of the command.

    repoDestinationPath

string

✓

Destination path used by “installRemoteRepo” task.

    repoRevision

string

✓

Repository revision used by “installRemoteRepo” task.

    repoType

“mcuxsdk_2.x” | “mcuxsdk” | “mcuxsdk_int” | “zephyr” | “zephyr_nxp” | “matter” | “matter_nxp”

✓

Repository type used by “installRemoteRepo” task.

    repoManifestFile

string

Manifest file used by “installRemoteRepo” task.

Command: "installRemoteStandalonePackage"

Properties supported by the “installRemoteStandalonePackage” command:

Property

Type

Required

Description

    command

“installRemoteStandalonePackage”

✓

ID of the command.

    packageDestinationPath

string

✓

Installation package path used by “installRemoteStandalonePackage” task.

    packageJsonFile

string

✓

JSON file name associated to the desired package used by “installRemoteStandalonePackage” task. See https://mcuxpresso.nxp.com/vscode/NXP.json for all the available packages.

    packageVersion

string

✓

Version of the package installed via “installRemoteStandalonePackage” task.

Command: "installLocalRepo"

Properties supported by the “installLocalRepo” command:

Property

Type

Required

Description

    command

“installLocalRepo”

✓

ID of the command.

    repoPath

string

✓

Path to the local repository used by “installLocalRepo” task.

Command: "installLocalArchive"

Properties supported by the “installLocalArchive” command:

Property

Type

Required

Description

    command

“installLocalArchive”

✓

ID of the command.

    archiveDestinationPath

string

✓

Archive installation path used by “installLocalArchive” task.

    archivePath

string

✓

Archive path used by “installLocalArchive” task.

Command: "installAchProduct"

Property

Type

Required

Description

    command

“installAchProduct”

✓

ID of the command.

    productID

string

✓

Remote ID of ACH product used by “installAchProduct” task.

    productName

string

✓

Product name used by “installAchProduct” task. Will be appended to “destinationPath”.

    destinationPath

string

✓

Product destination path used by “installAchProduct” task.

    toolchainPath

string

Toolchain path used by the “installAchProduct” task, required for non-Zephyr projects imported from ACH repository.

    zephyrSdkPath

string

Zephyr SDK path used by the “installAchProduct” task, required for Zephyr projects imported from ACH repository.

Command: "uninstallRepo"

Properties supported by the “uninstallRepo” command:

Property

Type

Required

Description

    command

“uninstallRepo”

✓

ID of the command.

    repoPath

string

✓

Path to the repository to uninstall.

    deleteFromDisk

boolean

Whether to delete repository from disk once task is executed. By default, repo is not deleted from disk.

Command: "importExampleFromRepo"

Properties supported by the “importExampleFromRepo” command:

Property

Type

Required

Description

    command

“importExampleFromRepo”

✓

ID of the command.

    importedProjectName

string

✓

Project name of the example imported using the “importExampleFromRepo” task.

    repoPath

string

✓

Path to the repository containing the example.

    repoTemplateID

string

✓

ID of the template example imported using the “importExampleFromRepo” task.

    appType

“inRepository” | “inWorkspace” | “freestanding” | “standalone”

✓

Application type to be created by the “importExampleFromRepo” task. See the official MCUXpresso for VS Code documentation to understand what type of projects can be created depending on the repository type.

    boardID

string

✓

Board ID used by the “importExampleFromRepo” task.

    exampleLocation

string

✓

Folder name for a workspace application, or the full path for freestanding and standalone applications. Used by the “importExampleFromRepo” task.

    toolchainPath

string

✓

Toolchain or Zephyr SDK path used by the “importExampleFromRepo” task.

    outOfTreeBoardsDir

string

Custom board folder used by “importExampleFromRepo” task.

Command: "importProject"

Properties supported by the “importProject” command:

Property

Type

Required

Description

    command

“importProject”

✓

ID of the command.

    projectDestinationPath

string

✓

Project destination path used by “importProject” task.

    projectPath

string

✓

Project path used by “importProject” task.

    repoPath

string

Repository path used by “importProject” task.

    toolchainPath

string

Toolchain or Zephyr SDK path used by “importProject” task.

Command: "createProject"

Properties supported by the “createProject” command:

Property

Type

Required

Description

    command

“createProject”

✓

ID of the command.

    projectName

string

✓

Name of the project created by the “createProject” task.

    destinationPath

string

✓

Path where the project will be created by the “createProject” task.

    boardID

string

*

Identifier of the board to create the project for. At least one of “boardID” or “deviceID” must be provided.

    deviceID

string

*

Identifier of the device to create the project for. At least one of “boardID” or “deviceID” must be provided.

    openConfig

boolean

Whether to open the configuration tool after the project is created. Default is false.

    repoPath

string

Path to an existing repository used by the “createProject” task. When provided, the provider type is inferred from it. At least one of “repoPath” or “repoType” must be provided.

    repoType

“Zephyr” | “MCUXpresso SDK”

Provider type of the repository used by the “createProject” task. When “repoPath” is not provided, the repository is cloned based on this type. When both are provided, they must be consistent. At least one of “repoPath” or “repoType” must be provided.

    toolchainPath

string

Toolchain path used by the “createProject” task, required for non-Zephyr projects. At least one of “toolchainPath” or “zephyrSdkPath” must be provided.

    zephyrSdkPath

string

Zephyr SDK path used by the “createProject” task, required for Zephyr projects. At least one of “toolchainPath” or “zephyrSdkPath” must be provided.

Command: "removeProject"

Properties supported by the “removeProject” command:

Property

Type

Required

Description

    command

“removeProject”

✓

ID of the command.

    projectName

string

✓

Project name used by “removeProject” task.

    deleteFromDisk

boolean

Whether to delete a project from the disk once a task is executed. By default, the project is not deleted.

    removeLinkedProjects

boolean

Whether to remove linked projects as well. By default, linked projects are removed. The “deleteFromDisk” property also applies to the way removal of linked projects is handled.

Command: "buildProject"

Properties supported by the “buildProject” command:

Property

Type

Required

Description

    command

“buildProject”

✓

ID of the command.

    projectName

string

✓

Project name used by “buildProject” task.

    buildConfigName

string

✓

Build configuration used by “buildProject” task.

    sysbuild

boolean

Set sysbuild enablement. By default, the enablement state is specified in the example/project definition at import/creation time.

    buildConfigOverride

object

Override settings used by “buildProject” task.

        boardID

string

Board ID.

        buildDir

string

Build directory.

        cmakeExtraArgs

string

Extra CMake arguments to be passed at build time.

        debugConsole

“default” | “semihost” | “uart” | “none”

Debug console type used by the application.

Command: "cleanProject"

Properties supported by the “cleanProject” command:

Property

Type

Required

Description

    command

“cleanProject”

✓

ID of the command.

    projectName

string

✓

Project name used by “cleanProject” task.

    buildConfigName

string

✓

Build configuration used by “cleanProject” task.

    sysbuild

boolean

Set sysbuild enablement. By default, the enablement state is specified in the example/project definition at import/creation time.

    buildConfigOverride

object

Override settings used by “cleanProject” task.

        boardID

string

Board ID.

        buildDir

string

Build directory.

        cmakeExtraArgs

string

Extra CMake arguments to be passed at clean time.

        debugConsole

“default” | “semihost” | “uart” | “none”

Debug console type used by the application.

Command: "rebuildProject"

Properties supported by the “rebuildProject” command:

Property

Type

Required

Description

    command

“rebuildProject”

✓

ID of the command.

    projectName

string

✓

Project name used by “rebuildProject” task.

    buildConfigName

string

✓

Build configuration used by “rebuildProject” task.

    sysbuild

boolean

Set sysbuild enablement. By default, the enablement state is specified in the example/project definition at import/creation time.

    buildConfigOverride

object

Override settings used by “rebuildProject” task.

        boardID

string

Board ID.

        buildDir

string

Build directory.

        cmakeExtraArgs

string

Extra CMake arguments to be passed at rebuild time.

        debugConsole

“default” | “semihost” | “uart” | “none”

Debug console type used by the application.

Command: "eraseFlash"

Properties supported by the “eraseFlash” command.

Property

Type

Required

Description

    command

“eraseFlash”

✓

ID of the command.

    projectName

string

✓

Project name used by “eraseFlash” task.

    probeSN

string

✓

Probe serial number to be used by the “eraseFlash” task.

    debugConfigName

string

Debug configuration name to be used by the “eraseFlash” task.

    debugConfigOverride

object

Override settings from debug configuration, used by the “eraseFlash” task.

Command: "programFlash"

Properties supported by the “programFlash” command.

Property

Type

Required

Description

    command

“programFlash”

✓

ID of the command.

    projectName

string

✓

Project name used by “programFlash” task.

    probeSN

string

✓

Probe serial number to be used by the “programFlash” task.

    baseAddressHex

string

Base address (hex format) for the file that will be programmed by the “programFlash” task.

    debugConfigName

string

Debug configuration name to be used by the “programFlash” task.

    debugConfigOverride

object

Override settings from debug configuration, used by the “programFlash” task.

    eraseAllFlash

boolean

Whether to erase all flash during execution of “programFlash” task.

    fileToProgram

string

Path to the binary/executable file to be programmed by the “programFlash” task.

    flashAllBuildImages

boolean

When true, all output targets of the selected project are programmed in sequence (equivalent to selecting Flash all build images in the Flash Programmer UI). The best available file format is chosen per domain using the priority: hex > bin > elf. Base addresses for binary files are resolved automatically from the project’s Kconfig build configuration. Cannot be combined with fileToProgram or baseAddressHex.

    resetTargetOnExecution

boolean

Whether to reset target after the completion of the “programFlash” task.

Command: "runDebugProject"

Properties supported by the “runDebugProject” command:

Property

Type

Required

Description

    command

“runDebugProject”

✓

ID of the command.

    projectName

string

✓

Project name used by “runDebugProject” task.

    probeSN

string

✓

Probe serial number to be used by the “runDebugProject” task.

    appOutputFile

string

Application output file path to be used by the “runDebugProject” task. By default, a temporary file is created.

    debugConfigName

string

Debug configuration name to be used by the “runDebugProject” task.

    debugConfigOverride

object

Override settings from debug configuration, used by the “runDebugProject” task.

    terminatePattern

string

Terminate pattern used by the “runDebugProject” task.

    terminateTimeout

number

Terminate timeout used by the “runDebugProject” task. By default, 60 seconds is the default timeout.

Command: "westBuild"

Properties supported by the “westBuild” command:

Property

Type

Required

Description

    command

“westBuild”

✓

ID of the command.

    projectName

string

Project name used by “westBuild” task. Not required when task is defined inside “tasks.json”.

    configPreset

string

Name of the config preset.

    configure

boolean

Whether to only configure the project. Default is false.

    pristine

“auto” | “always” | “never”

Pristine build folder setting. “auto” uses heuristics to determine if a pristine build is necessary, “always” forces a pristine build, “never” skips it.