Set up toolchain
This section contains the steps to install the necessary components required to build and run a MCUXpresso SDK demo application with the Arm GCC toolchain, as supported by the MCUXpresso SDK.
Install GCC Arm embedded toolchain
Download and run the installer from the GNU Arm Embedded Toolchain Downloads page. The GNU Arm embedded toolchain contains the GCC compiler, libraries, and other tools required for bare-metal software development. The GCC toolchain should correspond to the latest supported version, as described in the MCUXpresso SDK Release Notes for EVK-MIMX8ULP (document MCUXSDKIMX8ULPRN).
Note: See How to set up Windows/Linux host system for setting up Linux host before compiling the application.
Parent topic:Set up toolchain
Add a new system environment variable for ARMGCC_DIR
Create a new system environment variable and name it ARMGCC_DIR
. The value of this variable should point to the Arm GCC embedded toolchain installation path. For this example, the path is:
$ export ARMGCC_DIR=<path_to_GNUARM_GCC_installation_dir>
Parent topic:Set up toolchain
Parent topic:Linux OS host