Example application structure
This section describes how the various types of example applications interact with the other components in the MCUXpresso SDK. To get a comprehensive understanding of all MCUXpresso SDK components and folder structure, see MCUXpresso SDK API Reference Manual.
Each <board_name>
folder in the boards directory contains a comprehensive set of examples that are relevant to that specific piece of hardware. Although we use the hello_world
example (part of the demo_apps
folder), the same general rules apply to any type of example in the <board_name>
folder.
In the hello_world
application folder you see the following contents:
|
|
All files in the application folder are specific to that example, so it is easy to copy and paste an existing example to start developing a custom application based on a project provided in the MCUXpresso SDK.
Parent topic:MCUXpresso SDK board support package folders