Build an example application
The following steps guide you through opening the hello_world example application. These steps may change slightly for other example applications, as some of these applications may have additional layers of folders in their paths.
If not already done, open the desired demo application workspace. Most example application workspace files can be located using the following path:
<install_dir>/boards/<board_name>/<example_type>/<application_name>/iar
Using the i.MX 8M Mini EVK board as an example, the
hello_worldworkspace is located in:<install_dir>/boards/evkmimx8mm/demo_apps/hello_world/iar/hello_world.eww
Select the desired build target from the drop-down. For this example, select hello_world – flash_debug.
|

|
To build the demo application, click Make, highlighted in red in Figure 2.
|

|
The build completes without errors.
Rename the generated
hello_world.bintom4_flash.bin, then copy it to the uuu tool directory.
Parent topic:Run a flash target demo by UUU