This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Build an example application

To build an example application, follow these steps.

  1. Open the GCC Arm embedded toolchain command window. To launch the window on the Windows operating system, select Start -> Programs -> GNU Tools ARM Embedded <version> -> GCC Command Prompt.

    |

|

  1. Change the directory to the example application project directory, which has a path similar to the following:

    <install_dir>/boards/<board_name>/<example_type>/<application_name>/armgcc
    

    For this example, the exact path is:

    <install_dir>/boards/evkmimx8ulp/demo_apps/hello_world/armgcc
    
  2. Type build_debug.bat at the command-line or double-click the build_debug.bat file in Windows Explorer to perform the build. The output is as shown in Figure 2.

    |

|

Note: To run the application, see the Run an application using imx-mkimage.

Parent topic:Windows OS host