This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

MCUXpresso SDK DSP Enablement

The DSP-specific enablement is available inside the MCUXpresso SDK release package for RT500. The path is: <SDK_ROOT>/devices/MIMXRT595S/

Unified device and peripheral driver source code that compiled for both ARM and DSP cores.

Note: Only a limited subset of peripheral drivers and components are supported on the DSP.

<SDK_ROOT>/boards/evkmimxrt595/dsp_examples/

DSP example applications are available at:<SDK_ROOT>/middleware/multicore/rpmsg_lite/

Unified RPMsg-Lite multicore communication library, with porting layers for ARM and DSP cores. <SDK_ROOT>/middleware/dsp/audio_framework/

Xtensa Audio Framework (XAF) for DSP core

Parent topic:Install MCUXpresso SDK