This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Build an example application

Perform the following steps to build the hello_world example application.

  1. Open the desired demo application workspace. Most example application workspace files can be located using the following path:

    <install_dir>/boards/<board_name>/<example_type>/<application_name>/iar
    

    Using the FRDM-K32L2A4S hardware platform as an example, the hello_world workspace is located in:

    <install_dir>/boards/frdmk32l2a4s/demo_apps/hello_world/iar/hello_world.eww
    
  2. Select the desired build target from the drop-down menu. For this example, select the hello_world – debug target.

  3. To build the demo application, click the Make button highlighted in red below.

  4. The build completes without errors.

Parent topic:Run a demo application using IAR