This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Run a demo using Keil MDK/μVision {#GUID-C92BA576-991F-400B-A84D-F88210330334}

This section describes the steps required to build, run, and debug example applications provided in the MCUXpresso SDK. The hello_world demo application targeted for the LPCXpresso55S69 hardware platform is used as an example, although these steps can be applied to any demo or example application in the MCUXpresso SDK.