This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Enable MCUXpresso SDK DSP

The following DSP-specific enablements are available inside the MCUXpresso SDK release package for RT600.

  • 
    

<SDK_ROOT>/devices/MIMXRT685S/


    Unified device and peripheral driver source code that can be compiled for both Arm and DSP cores.

    **Note:** Only a limited subset of peripheral drivers and components is supported on the DSP.

-   ```
<SDK_ROOT>/boards/evkmimxrt685/dsp_examples/
DSP example applications
  • 
    

<SDK_ROOT>/middleware/multicore/rpmsg_lite/


    Unified RPMsg-Lite multicore communication library, with porting layers for Arm and DSP cores

-   ```
<SDK_ROOT>/middleware/dsp/audio_framework/
Xtensa Audio Framework \(XAF\) for DSP core
  • 
    

<SDK_ROOT>/middleware/dsp/audio_framework/libxa_af_hostless/


    Source code and documentation for the core XAF framework

-   ```
<SDK_ROOT>/middleware/dsp/audio_framework/testxa_af_hostless/
  • Utilities and tests for developing applications with the XAF framework

    <SDK_ROOT>/middleware/dsp/audio_framework/testxa_af_hostless/test/plugins
    
  • XAF components and codec binaries

  • 
    

<SDK_ROOT>/middleware/dsp/naturedsp/hifi4/


    NatureDSP Math Library for HiFi4 DSP


**Parent topic:**[Install MCUXpresso SDK](../topics/install_mcuxpresso_sdk.md)