This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Mini/micro USB cable

  • EVKB-IMXRT1050 board

  • Personal Computer

Board settings

Remove the resistor R334 and weld 0Ω resistor to R278,R279,R280,R281.

To make the example work, connections needed to be as follows:

       MASTER           connect to      SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J24-4                SIN       SW5-3
SIN        J24-5                SOUT      SW5-2
SCK        J24-6                SCK       SW5-1
PCS0       J24-3                PCS0      SW5-4

Prepare the Demo

  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

You can see the similar message shows following in the terminal if the example runs successfully.

LPSPI Master interrupt - FLEXIO SPI Slave edma dynamic transfer example start.
This example use one lpspi instance as master and one flexio spi slave on one board.
Master uses interrupt and slave uses edma way.
Master transfers indefinite amount of data to slave, and the CS signal remains low during transfer.
After master finishes the transfer and re-asserts the CS signal, interrupt is triggered to let user know.
Slave must configure the transfer size larger than master's.
Please make sure you make the correct line connection. Basically, the connection is:
LPSPI_master -- FLEXIO_SPI_slave
   CLK      --    CLK
   PCS      --    PCS
   SOUT     --    SIN
   SIN      --    SOUT
Slave received 128 bytes of data
Slave received 128 bytes of data
LPSPI master <-> FLEXIO SPI slave transfer all data matched!

End of Example.