This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Mini/micro USB cable

  • EVKB-IMXRT1050 board

  • Personal Computer

Board settings

This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.

Prepare the Demo

  1. Connect a USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the demo runs successfully, the log would be seen on the terminal like:

FLEXRAM ram allocate example.

Allocate on-chip ram:

   OCRAM bank numbers 4

   DTCM  bank numbers 4

   ITCM  bank numbers 8

Allocate on-chip ram success

OCRAM access to 0x20220000 boundary.

DTCM access to nearly 0x20020000 boundary.

ITCM access to nearly 0x40000 boundary.

FLEXRAM ram allocate example finish.