This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Mini/micro USB cable

  • EVKB-IMXRT1050 board

  • Personal Computer

Board settings

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

Note: LittleFS example built using arm-gcc does not work as expected out-of-the box. Other supported toolchains are not affected.

When the example runs successfully, you can see the similar information from the terminal as below.

SHELL (build: Feb 28 2018)
Copyright  2017  NXP
LFS>>