Hardware requirements
Mini/micro USB cable
EVKB-IMXRT1050 board
Personal Computer
SD card
Board settings
Please insert the SDCARD into card slot(J20) Note: If you want to use a SD3.0 card with SD3.0 protocol, just insert a SD3.0 card into the card slot will be ok.
Prepare the Demo
Connect a micro USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Insert SD card to card slot
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
SDCARD fatfs freertos example.
Card inserted.
Make file system......The time may be long if the card capacity is big.
Create directory......
TASK1: write file successed.
TASK2: write file successed.
TASK1: finsied.
TASK2: finsied.