This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Mini/micro USB cable

  • MIMXRT1170-EVKB board

  • Loopback network cable RJ45 standard

  • Network cable RJ45 standard

  • Network switch

  • Personal Computer

Board settings

If Rx frame CRC error occurs, try to populate a suitable C66. The REV C/C1 boards populate 22pF which is high and may result in CRC errors on some of boards, if this is the case C66 may be removed or replaced by a smaller capacitor.

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Insert loopback network cable into network switch device(support loopback frames) and connect switch to board’s Ethernet RJ45 port(J4).

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Note: If not use switch, only insert loopback network cable into Ethernet RJ45 port, auto-negotiation result is 100M. Here we use switch to test 1G.

Make loopback cable: Standard 1 Standard 2 J1 orange+white green+white J2 orange green J3 green+white orange+white J4 blue brown+white J5 blue+white brown J6 green orange J7 brown+white blue J8 brown blue+white

Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to the sheet above. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.

Running the demo

When the demo runs, the log would be seen on the terminal like:

ENET example start. The 1 frame transmitted success! A total of 1 frame(s) has been successfully received! The 2 frame transmitted success! A total of 2 frame(s) has been successfully received! The 3 frame transmitted success! A total of 3 frame(s) has been successfully received!

……

The 20 frame transmitted success! A total of 20 frame(s) has been successfully received!