This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • MIMXRT1170-EVKB board

  • JLink Plus

  • 5V power supply

  • Personal Computer

  • RK055MHD091 panel or RK055AHD091 panel or RK055IQH091 panel or RaspberryPi panel

  • SD card

Board settings

  1. Connect the panel to J48. For RaspberryPi panel, connect the panel to J84, then connect the panel’s 5V pin to J85-1, GND pin to J85-2.

  2. Prepare the H264 files and save in SD card.

  3. Please make sure R136 is weld for GPIO card detect.

  4. Insert the SDCARD into card slot(J15).

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Build the project, the project uses RK055MHD091 by default, to use other panels, change #define DEMO_PANEL DEMO_PANEL_RK055MHD091 to #define DEMO_PANEL DEMO_PANEL_RK055IQH091 or #define DEMO_PANEL DEMO_PANEL_RK055AHD091 or #define USE_MIPI_PANEL DEMO_PANEL_RASPI_7INCH in display_support.h.

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

If this example runs correctly, pictures are shown in the lcd panel.