Hardware requirements
Micro USB cable
MIMXRT1170-EVKB board
JLink Plus
5V power supply
Personal Computer
RK055MHD091 panel or RK055AHD091 panel or RK055IQH091 panel or RaspberryPi panel
SD card
Board settings
Connect the panel to J48. For RaspberryPi panel, connect the panel to J84, then connect the panel’s 5V pin to J85-1, GND pin to J85-2.
Unzip the pics.zip, place the png pictures to the SD card.
Please make sure R136 is weld for GPIO card detect and then insert the SDCARD into card slot(J15).
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Build the project, the project uses RK055MHD091 by default, to use other panels, change #define DEMO_PANEL DEMO_PANEL_RK055MHD091 to #define DEMO_PANEL DEMO_PANEL_RK055IQH091 or #define DEMO_PANEL DEMO_PANEL_RK055AHD091 or #define USE_MIPI_PANEL DEMO_PANEL_RASPI_7INCH in display_support.h.
Insert SD card to card slot
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
If this example runs correctly, pictures are shown in the lcd panel one by one.