This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Mini/micro USB cable

  • MIMXRT1170-EVKB board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a USB cable between the PC host and the OpenSDA USB on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, following information can be seen on the OpenSDA terminal:


==FlexCAN loopback functional example -- Start.==

Send message from MB8 to MB9
tx word0 = 0x0
tx word1 = 0x1
tx word2 = 0x2
tx word3 = 0x3
tx word4 = 0x4
tx word5 = 0x5
tx word6 = 0x6
tx word7 = 0x7
tx word8 = 0x8
tx word9 = 0x9
tx word10 = 0xa
tx word11 = 0xb
tx word12 = 0xc
tx word13 = 0xd
tx word14 = 0xe
tx word15 = 0xf

Received message from MB9
rx word0 = 0x0
rx word1 = 0x1
rx word2 = 0x2
rx word3 = 0x3
rx word4 = 0x4
rx word5 = 0x5
rx word6 = 0x6
rx word7 = 0x7
rx word8 = 0x8
rx word9 = 0x9
rx word10 = 0xa
rx word11 = 0xb
rx word12 = 0xc
rx word13 = 0xd
rx word14 = 0xe
rx word15 = 0xf

==FlexCAN loopback functional example -- Finish.==