This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • evkbmimxrt1170 board

  • Personal Computer

  • Embedded Artists 1XK M.2 Module (EAR00385) - direct M2 connection.

  • Embedded Artists 1ZM M.2 Module (EAR00364) - direct M2 connection.

Jumper settings for RT1170-EVKB (enables external 5V supply):

remove J38 5-6 connect J38 1-2 connect J43 with external power(controlled by SW5)

Murata Solution Board settings

Embedded Artists M.2 module resource page: https://www.embeddedartists.com/m2 Embedded Artists 1XK module datasheet: https://www.embeddedartists.com/doc/ds/1XK_M2_Datasheet.pdf Embedded Artists 1ZM module datasheet: https://www.embeddedartists.com/doc/ds/1ZM_M2_Datasheet.pdf

The hardware should be reworked according to the Hardware Rework Guide for MIMXRT1170-EVKB and Murata 1XK M.2 Adapter in document Hardware Rework Guide for EdgeFast BT PAL. The hardware should be reworked according to the Hardware Rework Guide for MIMXRT1170-EVKB and Murata 1ZM M.2 Adapter in document Hardware Rework Guide for EdgeFast BT PAL.

Note: To ensure that the LITTLEFS flash region has been cleaned, all flash sectors need to be erased before downloading example code. After downloaded binary into qspiflash and boot from qspiflash directly, please reset the board by pressing SW4 or power off and on the board to run the application.