Hardware requirements
Micro USB cable
MIMXRT1060-EVKC board
JLink Plus
5V power supply
Personal Computer
RK043FN02H-CT or RK043FN66HS-CT6 LCD board (RK043FN02H-CT and RK043FN66HS-CT6 are compatible)
SD card
Board settings
Connect the RK043FN02H-CT or RK043FN66HS-CT6 to board.
Prepare the H264 files and save in SD card.
Insert the SDCARD into card slot.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
If this example runs correctly, pictures are shown in the lcd panel.