This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Mini/micro USB cable

  • MIMXRT1060-EVKC board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the ocotp example in the terminal window:

OCOTP Peripheral Driver Example

OCOTP controller version: 0x06000000

Note: To download binary into qspiflash and boot from qspiflash directly, following steps are needed:

  1. Compile flash target of the project, and get the binaray file “ocotp_example.bin”.

  2. Set the SW7: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J33.

  3. Drop the binaray into disk “RT1060-EVK” on PC.

  4. Wait for the disk disappear and appear again which will take couple of seconds.

  5. Reset the board by pressing SW7 or power off and on the board.