This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • evkcmimxrt1060 board

  • Personal Computer

  • Embedded Artists 2EL M.2 Module (Rev-A1) - direct M2 connection.

Board settings

Before building the example application select Wi-Fi module macro in the app_bluetooth_config.h. (see #define WIFI_BOARD). If you want to use Embedded Artists 2EL M.2 Module(Rev-A1), please change the macro to WIFI_IW612_BOARD_MURATA_2EL_M2.

Jumper settings for RT1060-EVKC (enables external 5V supply):

remove J40 5-6 connect J40 1-2 connect J45 with external power(controlled by SW6) remove J110 jumper cap remove R196,R201,R213,R211 connect J110-1(GPT2_CLK) to R2140(SAI_MCLK) connect ENET_MDIO(GPT2_CAP1) with J97(SAI_SW) connect ENET_MDC(GPT2_CAP2) with 2EL’s GPIO_27(Sync Signal)

Murata Solution Board settings

Embedded Artists 2EL module datasheet: https://www.embeddedartists.com/doc/ds/2EL_M2_Datasheet.pdf

The hardware should be reworked according to the hardware rework guide for evkcmimxrt1060 and Murata 1ZM M.2 Adapter in document Hardware Rework Guide for EdgeFast BT PAL.

Note: To ensure that the LITTLEFS flash region has been cleaned, all flash sectors need to be erased before downloading example code. After downloaded binary into qspiflash and boot from qspiflash directly, please reset the board by pressing SW7 or power off and on the board to run the application.