Hardware requirements
Mini/micro USB cable
Target microcontroller board
Personal Computer
FreeMASTER 3.1.3 with Network plug-in updated for Segger RTT communication
Board settings
No special settings are required. By default this demo communicates over a SEGGER J-Link interface of the debugger USB connection.
Prepare the demo
Connect a USB cable between the host PC and the Debug USB port on the target board.
Compile and download the program to the target microcontroller.
Run and resume application execution when debugger stops in the main() function.
Connect with FreeMASTER
Run FreeMASTER, use the Connection Wizard or open Project Options.
Select network communication and configure the plug-in for RTT protocol.
Start communication, FreeMASTER loads the initial TSA Active Content links in the Welcome page.
Click the “FreeMASTER Demonstration Project (embedded in device)” in the Welcome page.
The demo is now running, you should be able to watch variable values and graphs.
More information
Read more information about FreeMASTER tool at http://www.nxp.com/freemaster. Feel free to ask questions and report issues at FreeMASTER’s community page at https://community.nxp.com/community/freemaster