This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • EVK-MIMX8M Plus board

  • J-Link Debug Probe

  • 12V power supply

  • Personal Computer

Board settings

Use Oscilloscope to measure and observe the Test Point J21-32 output signal.

Prepare the Demo

  1. Connect 12V power supply and J-Link Debug Probe to the board, switch SW3 to power on the board

  2. Connect a USB cable between the host PC and the J23 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the demo.

Running the demo

These instructions are displayed/shown on the terminal window:

PWM driver example.