This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • two MIMX8ULP-EVK/EVK9 board

  • JLink Plus

  • 5V power supply

  • Personal Computer

Board settings

populate J8 for two boards. The example requires connecting between CAN pins of two boards. The connection should be set as follows:

Between two boards:

  • J8-1(CANH) node A, J8-1(CANH) node B

  • J8-2(CANL) node A, J8-2(CANL) node B

  • J8-3(GND) node A, J8-3(GND) node B

Prepare the Demo

  1. Connect 5V power supply and JLink Plus to the board, switch SW10 to power on the board

  2. Connect a micro USB cable between the host PC and the J17 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, following information can be seen on the terminal:

This message displays on the node A terminal:

FlexCAN pretended networking wake up example.
Please select local node as A or B:
Note: Node B should start first.
Node:a
Press any key to trigger one-shot transmission
Send message ID: 0x123, payload: 0x0055000000000000

Press any key to trigger the next transmission!
Send message ID: 0x123, payload: 0x0155000000000000

Press any key to trigger the next transmission!
Send message ID: 0x125, payload: 0x0255000000000000

Press any key to trigger the next transmission!
Send message ID: 0x125, payload: 0x0355000000000000

Press any key to trigger the next transmission!
Send message ID: 0x123, payload: 0x0455000000000000

Press any key to trigger the next transmission!
Send message ID: 0x123, payload: 0x0056000000000000

...

This message displays on the node B terminal:

FlexCAN pretended networking wake up example. Please select local node as A or B: Note: Node B should start first. Node:b Note B will enter lower power mode and wake up until received 4 specific messages. Wake up message format: Standard (11 bit id) Wake up message ID range: 0x123 to 0x124 Wake up payload range : 0x0055000000000000 to 0x0056000000000000 Waken up! Match message 0 ID: 0x123, payload: 0x0055000000000000 Match message 1 ID: 0x123, payload: 0x0155000000000000 Match message 2 ID: 0x123, payload: 0x0455000000000000 Match message 3 ID: 0x123, payload: 0x0056000000000000 Enter lower power mode again!