Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1010 board
Personal Computer
Board settings
LPUART one board: Using instance 4 of LPUART interface to transfer data to itself. TX pin is connected with RX pin.
LPUART4 CONNECTS TO LPUART4
Pin Name Bard Location Pin Name Bard Location
TXD J26-12 RXD J26-10
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
LPUART 9-bit mode example begins
LPUART is configured with address, only data sent to itself after matched address can be received
LPUART will send first piece of data out:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
LPUART will address itself
LPUART will send the other piece of data out:
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
LPUART received data:
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
All data matches!