Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1010 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the ocotp example in the terminal window: For flash target:
OTFAD example started!
Hitted context: 0x0
Erasing Serial NOR over FlexSPI...
Erase sector finished !
Decrypted data - successfully.
For ram target:
OTFAD example started!
Hitted context: 0x0
Erasing whole chip over FlexSPI...
Erase whole chip finished !
Erasing Serial NOR over FlexSPI...
Erase sector finished !
Decrypted data - successfully.
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.
Note: To generate ciphertext, you can use OTFAD_GetEncryptedCounter() and OTFAD_EncryptData() API in example[selected] or other library.
use OTFAD_GetEncryptedCounter() API get encrypted counter.
use encrypted counter XOR plaintext to generate ciphertext.