This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Mini/micro USB cable

  • EVK-MIMXRT1010 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

These instructions are displayed/shown on the terminal window:

******** System Start ********
System reset by: Power On Reset!

- 1.Testing System reset by software trigger.
******** System Start ********
System reset by: Software Reset!

- 2.Testing system reset by WDOG timeout.
--- wdog Init done---

******** System Start ********
System reset by: Time Out Reset!

- 3.Test the WDOG refresh function by using interrupt.
--- wdog Init done---

WDOG has be refreshed!
WDOG has be refreshed!
WDOG has be refreshed!

~~~~~~~~~~~~~~~~~~~~~

Note:
To debug in qspiflash, following steps are needed:
1. Select the flash target and compile.
2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.
3. Start debugging in IDE.
   - Keil: Click "Download (F8)" to program the image to qspiflash first then clicking "Start/Stop Debug Session (Ctrl+F5)" to start debugging.