This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Mini/micro USB cable

  • EVK-MIMXRT1020 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

These instructions are displayed/shown on the terminal window:

Starting channel No.0 ...
 Channel No.0 interrupt is occurred !
 Channel No.0 interrupt is occurred !
 Channel No.0 interrupt is occurred !
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
And you will find the user LED is taking turns to shine.

Note:
To debug in qspiflash, following steps are needed:
1. Select the flash target and compile.
2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.
3. Start debugging in IDE.
   - Keil: Click "Download (F8)" to program the image to qspiflash first then clicking "Start/Stop Debug Session (Ctrl+F5)" to start debugging.