This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Mini/micro USB cable

  • MIMXRT1040-EVK board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

RNGA Peripheral Driver Example Generate 10 random numbers: Random[0] = 0xE1554295 Random[1] = 0x827AD456 Random[2] = 0x9A1CBE1E Random[3] = 0x4354CB53 Random[4] = 0xFE3B2494 Random[5] = 0xEDAB3F7D Random[6] = 0x9AB91722 Random[7] = 0x4F54D999 Random[8] = 0x492414D1 Random[9] = 0x84611992

Press any key to continue…