This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Mini/micro USB cable

  • MIMXRT1040-EVK board

  • Personal Computer

  • SD card

Board settings

Please insert the SDCARD into card slot Note: If you want to use a SD3.0 card with SD3.0 protocol, just insert a SD3.0 card into the card slot will be ok. As the EVK board limitaion, there is eletronic mux added for switch between M.2 and sdcard which will affect the sdcard SDR104 timing. So the maximum sd card timing frequency been decreased to 100MHZ to improve the stability. User can remove the limitation by change the macro BOARD_SDMMC_SD_HOST_SUPPORT_SDR104_FREQ in sdmmc_config.h from (100000000U) to (200000000U).

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Insert SD card to card slot

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the terminal like:


FATFS example to demonstrate how to use FATFS with SD card.

Please insert a card into board.
Detected SD card inserted.

Makes file system......This time may be long if the card capacity is big.

Creates directory......

Creates a file in that directory......

Lists the file in that directory......
General file : F_1.DAT.
Directory file : DIR_2.

Writes/reads file until encounters error......

Writes to above created file.
Reads from above created file.
Compares the read/write content......
The read/write content is consistent.
Input 'q' to quit read/write.
Input other char to read/write file again.