This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Mini/micro USB cable

  • MIMXRT1160-EVK board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as shown below.

Welcome to the BUBBLE example

You will see the change of LED brightness when change angles of board

x=  6 y = 22
x=  8 y = 26
x= 10 y = 28
x= 10 y = 28
x= 11 y = 29
x= 11 y = 29

Note:

  • If the user LED flashes constantly and the following message is printed on the console: Sensor device initialize failed!

    Please check the sensor chip U34

    please check if the combo sensor (U34) is presented on the board.