Hardware requirements
Mini/micro USB cable
MIMXRT1160-EVK board
Personal Computer
RK055AHD091 panel or RK055MHD091 panel
OV5640 camera
Board settings
Connect the panel to J48 Connect camera to J2 Connect 5V power to J43, set J38 to 1-2
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Build the project, this project uses RK055MHD091 panel by default, to use the RK055AHD091 panel, change #define DEMO_PANEL DEMO_PANEL_RK055MHD091 to #define DEMO_PANEL DEMO_PANEL_RK055AHD091 in display_support.h.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs, the screen shows the camera input frame.