Hardware requirements
Mini/micro USB cable
MIMXRT1160-EVK board
Headphone(OMTP standard)
Personal Computer
Board settings
J33, headphone connected
connect FLEXIO pins to the pad as follows:
Pin Name Board Location Pin Name Board Location
RX_DATA J26-2 RX_DATA J61-2
TX_DATA J26-4 TX_DATA J62-2
SYNC J26-6 SYNC J59-2
BCLK J26-8 BCLK J60-2
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
Note: This demo uses both headphone mic and board main mic(P1) as input source. The headphone mic provides left channel data, and main mic (P1) provides right channel data. If users found there is noise while do record operation, most probably it is the headphone standard issue (OMTP and CTIA standard difference). You should use the OMTP standard headphone. You can disable the left channel by using an headphone without microphone feature.
When the demo runs successfully, the log would be seen on the OpenSDA terminal like as below.
~~~~~~~~~~~~~~~~~~~~~
FLEXIO I2S EDMA example started!
FLEXIO I2S EDMA example finished!
~~~~~~~~~~~~~~~~~~~~~