This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Mini/micro USB cable

  • EVK-MIMXRT1160 board

  • Personal Computer

  • SD card

Board settings

Please make sure R136 is weld for GPIO card detect.

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Insert SD card to card slot

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the terminal like:


Card size xxxxx bytes

Working condition:

  Voltage : xxxV

  Timing mode: xxx

  Freq : xxx HZ

Read/Write/Erase the card continuously until encounter error......

Write/read one data block......
Compare the read/write content......
The read/write content is consistent.
Write/read multiple data blocks......
Compare the read/write content......
The read/write content is consistent.
Erase multiple data blocks......

Input 'q' to quit read/write/erase process.
Input other char to read/write/erase data blocks again.