Hardware requirements
Micro USB cable
Two MIMXRT1180-EVK boards
Personal Computer
Board settings
Weld 1.5kΩ to R778 I3C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of I3C interface, I3C2 pins of MASTER_BOARD are connected with I3C2 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
I3C2_CLK J50-1 I3C2_CLK J50-1
I3C2_SDA J50-2 I3C2_SDA J50-2
GND J50-4 GND J50-4
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following message shows in the terminal if the example runs successfully.
I3C board2board EDMA example -- Master transfer.
Master will send data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
I3C master do dynamic address assignment to the I3C slaves on bus.
I3C master dynamic address assignment done.
Start to do I3C master transfer in I3C SDR mode.
I3C master wait for slave IBI event to notify the slave transmit size.
I3C master received slave IBI event, data size 1, value 0x20.
I3C master transfer successful in I3C SDR mode.
~~~~~~~~~~~~~~~~~~~~~~~~~~~