Hardware requirements
Mini/micro USB cable
Two MIMXRT1180-EVK board
Personal Computer
Board settings
Remove R79, R80 LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C2 pins of MASTER_BOARD are connected with LPI2C2 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C2_SCL J44-20 LPI2C2_SCL J44-20
LPI2C2_SDA J44-18 LPI2C2_SDA J44-18
GND J44-19 GND J44-19
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .