Hardware requirements
MIMXRT1180-EVK RevC
FRDM-MC-LVPMSM
Teknic2311P Motor
RJ45 Network cable
Mini/micro USB cable
Personal Computer on which the TwinCat3 has been installed
Board settings
Board needs to rework, please refer to ‘.\docs\ecatServoMotor\eCAT_Servo_Motor_Example_User_Guide.pdf’ to rework board.
Prepare the Demo
Generate the SSC source code
Download Slave Stack Code Tool(SSC Tool) from BECKHOFF official website and install it
Open Slave Stack Code Tool
Click ‘File’ -> ‘New’ -> ‘Import’ to import the Congfig file Select servo_motor.xml under path ‘.\boards\evkmimxrt1180\ecat_examples\servo_motor<core>\SSC’.
Click ‘Project’ -> ‘Create new Slave Files’ ‘Source Folder’(default): ‘.\boards\evkmimxrt1180\ecat_examples\servo_motor<core>\SSC\Src’. Click ‘Start’.
Copy SSC souce code to ‘.\boards\evkmimxrt1180\ecat_examples\servo_motor<core>\SSC\Src’, and change to ‘.\boards\evkmimxrt1180\ecat_examples\servo_motor<core>\SSC’ path to apply the patch. Linux: 1. Download dos2unix command apt-get install dos2unix 2. Transfer SSC source code format dos2unix Src/* 3. Apply patch patch -d Src < CiA402-combine-the-SSC-slave-with-ec_pmsm-support.patch Windows: 1. Download patch.exe and Unix2Dos.exe tool Download Windows Patch Utility from http://gnuwin32.sourceforge.net/downlinks/patch-bin-zip.php . Download Dos2Unix/Unix2Dos-Text file format converters from https://sourceforge.net/projects/dos2unix/ . 2. Transfer the patch format $(Dos2Unix/Unix2Dos-DIR)/bin/unix2dos.exe CiA402-combine-the-SSC-slave-with-ec_pmsm-support.patch 3. Apply patch patch.exe -i CiA402-combine-the-SSC-slave-with-ec_pmsm-support.patch -d ./Src
Connect FRDM-MC-LVPMSM board Connect the Teknic2311P motor to FRDM-MC-LVPMSM board and connect FRDM-MC-LVPMSM board to MIMXRT1180-EVK board.
Connect EtherCAT Port0 with TwinCAT3 RJ45 interface labeled as J28 is the EtherCAT Port0.
Connect a USB cable between the host PC and the OpenSDA USB port on the target board
Open a serial terminal with the following settings
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo
Update ESI file to EEPROM
Copy ESI file ‘ECAT-SERVO-MOTOR.xml’ generated by SSC TOOL to <TwinCAT_installation_folder>/
/Config/io/EtherCAT/ Restart TwinCAT3 IDE
Scan device and Update EEPROM
Scan and load this device
Activate configuration and start motor control