This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • EVK-MIMXRT595 board

  • Personal Computer

Board settings

  • Keep JTAG pins open, don’t connect any debugger on it.

  • For low power purpose, the demo requires pad voltage supply to be fixed as follows: VDDIO_0: 1.8V (PMIC SW2_OUT using default setting 1.8V) VDDIO_1: 1.8V (PMIC SW2_OUT using default setting 1.8V) VDDIO_2: 1.8V (PMIC SW2_OUT using default setting 1.8V) VDDIO_3: 3.3V (PMIC LDO2_OUT using default setting 3.3V) VDDIO_4: 1.8V (PMIC SW2_OUT using default setting 1.8V) NOTE: Supplying wrong voltage on the pads is harmful to the device.

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows in the terminal window:

Power Manager Demo.
The "user key" is: SW2
Select an option
        1. Sleep mode
        2. Deep Sleep mode
        3. Deep power down mode
        4. Full deep power down mode
/* Type in '1' in terminal */
Entering Sleep [Press the user key to wakeup] ...
/* Push SW2 */
Pin event occurs
Wakeup.
Select an option
        1. Sleep mode
        2. Deep Sleep mode
        3. Deep power down mode
        4. Full deep power down mode
/* Type in '2' in terminal */
Entering Deep Sleep [Press the user key to wakeup] ...
/* Push SW2 */
Pin event occurs
Wakeup.
Select an option
        1. Sleep mode
        2. Deep Sleep mode
        3. Deep power down mode
        4. Full deep power down mode
/* Type in '3' in terminal */
Entering Deep Powerdown [Reset to wakeup] ...
Press any key to confirm to enter the deep power down mode and wakeup the device by reset.
/* Type in any character to really run into deep power down */
/* Push reset button on board */
Board wake up from deep or full deep power down mode.
Power Manager Demo.
The "user key" is: SW2
Select an option
        1. Sleep mode
        2. Deep Sleep mode
        3. Deep power down mode
        4. Full deep power down mode